STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Interfacing with MEMS digital microphone

Hello,I'm using an stm32l151re to interface with mp34dt05-a mems microphone. I'm using it to determine noise level. The communication between smt32 mcu and the sensor is based on I2S protocol with dma. My issue is that my project consists of multiple...

Problems with the PDM2PCM-Lib and a STM32L151

I'm having problems with the PDM2PCM lib and am getting desperate.I have a STM32L151 with an external clock source of 8.192 MHz. The SYSCLK runs with 16.384 MHz. The APB2 (SPI1) runs with 4.096 MHz.I'm sampling a PDM mic with an 8-bit SPI at 2.048 MH...

bub by Associate
  • 216 Views
  • 0 replies
  • 0 kudos

Using PDM to PCM conversion library

I am using a STM32L1 MCU and I want to use the PDM to PCM conversion library, so I downloaded X-CUBE-MEMSMIC1, in the audio PDM lib folder I found libPDMFilter_CM3_Keil.lib. In the release note I read this lib is for 16KHz PCM data sampling rate, So ...

J Lee by Associate III
  • 610 Views
  • 4 replies
  • 0 kudos