STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I am using a STM32F7676vit6 Controller an try to set up a SAI connection to my audio CODEC now my problem is that the CODEC has two Serial outputs and one serial input.

Hey, I am using a STM32F7676vit6 Controller an try to set up a SAI connection to my audio CODEC now my problem is that the CODEC has two Serial outputs and one serial input. So i configured:SAI1A to be the transmitting master SAI1B is a synchronous S...

LFrei.2 by Associate
  • 258 Views
  • 2 replies
  • 0 kudos

Resolved! SAI_AudioPlayback example with ArmClang

Hi,i tried the SAI_AudioPlayback example for the h745 discovery board. I'm using Keil and with the keil 5 armcc compiler everything works fine.Now i switched to armclang 6 and replaced the "libPDMFilter_cm7_keil_wc16.lib" with "libPDMFilter_cm7_gcc_w...

Jnevi.1 by Senior
  • 1762 Views
  • 12 replies
  • 0 kudos

How to Use BSP Library for Audio Recording?

I'd like to create a program by which I can record and listen sound by using my board, STM32F746G-Disco. I'd like to use BSP library, however, I have some questions.When I looked at the stm32746g_discovery_audio.c file, I saw that there are 2 global ...

Resolved! Question about frame format of sai

Hi,​I'm implementing signal processing code.(cs42l51 audio in --> stm32 --> cs42l51 audio out)And i'm using STM32H7B3-discovery kit.I have some question about frame format of sai and cs42l51.When i send sine wave data from stm32 to cs42l51, the wavef...

0693W00000LyqwpQAB.png 0693W00000LyqxnQAB.png 0693W00000LyqzKQAR.png
Younjun by Associate II
  • 914 Views
  • 7 replies
  • 0 kudos