MCU boot for STM32H743
Hello Techies, We are using STM32H743, we would like to run mcuboot on stm32h743, but we haven't find the example for stm32h7xx devices, Is there any specific reason not to provide mcuboot example for h7 devices?
Hello Techies, We are using STM32H743, we would like to run mcuboot on stm32h743, but we haven't find the example for stm32h7xx devices, Is there any specific reason not to provide mcuboot example for h7 devices?
I've worked out how to disable in the MEMs microphone I just want to use the blue 3.5mm input to receive/record the incoming audio. Thanks.
I'm trying to receive SPDIF data using an STM32F446RET using PB7 as SPDIFRX. The signal itself is perfect, a clear and sharp waveform can be seen directly at the input pin. The whole stuff is configured in CubeMX which also generated the code for int...
There is a new Digital Power software expansion pack for STM32Cube, X-CUBE-DPOWER.https://www.st.com/en/embedded-software/x-cube-dpower.html.Does anyone know if the default code generated will immediately work on STEVAL-ISA172V2?https://www.st.com/en...
When my STM32G0B1KET receives an Discover SVIDs message, it responds GOODCRC, then the core library function PE_StateMachine_VDM() calls the reset handler. After reset the system hardfaults. System responds to discover identity properly. The USBPD_VD...
Hi all,I'm doing some research about STLs. What is different between STM's X-CUBE-STL offering and ARM STL Libraries ? Why would you use one over another ?Thank you, best regards
Hello Community,I'm working on stm32u5(B-U585I-IOT02A). B-U585I-IOT02A has two digital mics, and St officially has an example of BSP to record audio.So after taking references from: https://github.com/STMicroelectronics/STM32CubeU5/blob/main/Projects...
Hello, I am looking to include USB audio streaming, this package looks perfect for handling a lot of the functionality. Just wondering if there are any guides on how to add this to a .ioc STM32CubeIde project for a different part than those in the Ex...
/** * @brief Read the Rx paysize * @rmtoll TX_PAYSZ TXPAYSZ LL_UCPD_ReadRxPaySize * @param UCPDx UCPD Instance * @retval RXPaysize. */ __STATIC_INLINE uint32_t LL_UCPD_ReadRxPaySize(UCPD_TypeDef const *const UCPD...
I have tried the application "STM32G474_MB1303_DRP_ONLY" from STUSB014-v1.1.1 to start my development. but there is a build break by some function in usbpd_core.h.But the related files and libraries are included in my project and listed in the projec...