Resolved! What documents to read to make 2 DRP 100w PD ports with stm32G071CBU3
I'm trying to make 2 DRP 100w ports but I can't find many related resources. Can anyone help by providing a sample code or related resources.
I'm trying to make 2 DRP 100w ports but I can't find many related resources. Can anyone help by providing a sample code or related resources.
Hello, I am developing a home appliance application on an MCU STM32G070CB using X-CUBE-CLASSB package and IAR EWARM IDE V8.32.4. I used NUCLEO-G070RB for the early development. The app ran fine until I turned on the SRAM parity check in the options b...
Hello, I'm able to connect the STM32CubeMonitor-UCPD with NUCLEO-G071RB and X-NUCLEO-SNK1M after following the instructions in AN5418. I only changed port 0 Sink PDO1 to 0x020641F4.I want to use the setup as a sink and always want to get the maximum ...
Hi, I am implementing a system with two DRP ports using an stm32g0 runnig a full USBPD stack. One of the ports is connected to a powerbank (usb pd v2). The other is connected to either a charger, which is used to power the system and charge the power...
Hello, I find there are a note for 'GP' version LQFP64 package.In blank of UCPD, which has the number "1" .The note is: One port with only one CC Line available(supporting limited number of use cases).Is that mean only one UCPD controller( UCPD1 or U...
The background is I am trying to build a pass through or charge through dongle like application. Using a G0 with 2 UCPD ports, port 0 as sink, and port 1 as DRP, using the respective TCPP chipsMy goal is to have the input port 0, get the available PD...
Hi everyone, We are developing safety device which need to go in a fail safe mode in any kind of failure to achieve SIL2 or SIL3 level of safety. And we want achieve UL certification.And we are using STM32G0B1CBTx MCU. And for writing code I am refer...
Initially I followed the tutorial at https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Getting_started_with_USB-Power_Delivery_Sink#-5BOPTIONAL-5D_Advanced_USB-PD_application but couldn't get that to work. It shows negotiations in the STM UCPD softwa...
Hi,We try to implement a DRP device with the USBPD library on a STM32G071 uC.From the documentation the requirements for the following functions are not clear:BSP_USBPD_PWR_VBUSOff():- Should it block until VBUS < USBPD_PWR_LOW_VBUS_THRESHOLD?- What ...
Hi All, I designed my board with a STM32G0 series MCU with the main intention of using its USB-PD peripheral. I later realized that it is only the STM32G0x1 series MCUs would be capable of USB-PD while I will be receiving a board turn with an STM32G0...