STM32 MCUs Other solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! USBX custom class

I'm developing firmware on a G0-family device.  I've implemented a CDC-ACM device based on one of the USBX sample applications.  Windows finds it, enumerates it and I can open it as a COM port.  That's all working.Now I want to add a second interface...

grahamm by Associate II
  • 850 Views
  • 3 replies
  • 2 kudos

DRD Settings for NUCLEO-G071RB and X-NUCLEO-DRP1M1

I would like to use NUCLEO-G071RB and X-NUCLEO-DRP1M1 to Source,UFP my USB devicesWhen the USB device side is set as Source, the role of data is DFP.​I used the DR SWAP command to change from DFP to UFP.But there was no sample code in x-cube-tcpp_v4....

forst by Associate III
  • 428 Views
  • 1 replies
  • 0 kudos