User Activity

Hey allI am building an application using a STM32G071RB with a DRP1M1 as ucpd 0 and a USBDP1 (old SNK1M1) as ucpd 1 and new to the STM UCPD worldIn an attempt to start from a working base, I used the DRP1M1_DRP example project as a starting point. Th...
I am trying to build an application with a SNK and DRP usbc port, using a USBPDM1 and a DRP1M1 with a nucleo g071rbI have successfully run the DRP example application, but when I try and add the functionality to my sink application stm32cubemonitor-u...
The background is I am trying to build a pass through or charge through dongle like application. Using a G0 with 2 UCPD ports, port 0 as sink, and port 1 as DRP, using the respective TCPP chipsMy goal is to have the input port 0, get the available PD...
I am curious if the STM32G0x1 can manage a DRP and a UFP USB-C as a charge through application?The USBPDM1 doc mentions other IC's and possibly other breakout boards.Is there a timline on when the TCPP03-M20 and documentation will be available?Cheers...
Hey STI am building an application that has two power sources, one USB-C (27W) with the STUSB4500 controller, and an optional DC input.Because the GPIO or attach pins can be open drain, theoretically they could be used to contrl a second FET on the p...
Kudos from