cancel
Showing results for 
Search instead for 
Did you mean: 

Are there CubeIDE projects for examples in S2-LP DK?

I see that all examples are for IAR or KEIL IDE.

Can you provide CubeIDE projects as well?

Regards,

Piotr Romaniuk

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Winfred LU
ST Employee

Hi Winfred,

thank you for the comprehensive migration guide. I found there some new information.

In general, I know the step needed for porting, but this is some extra work to be done.

It would be nice to have a version of project for IDE that is owned by ST (currently it is CubeIDE, TrueStudio is deprecated).

Of course we know advantages of IAR Workbench and KEIL IDE, but I'd rather expect that I also found in DK the example of source code that run on ST IDE.

The DK source code is 2 years old, so maybe it is good idea for ST to add project files for CubeIDE as well?

In my opinion this problem is common for many engineers that would like to evaluate Spirit2-LP chip, and the need of porting can discourage them.

Regards,

Piotr Romaniuk

PS

By the way, on which IDE were built binaries in DK?

chrisferrero
Associate

Hi Piotr,

Did you manage to import the IAR project into CubeIDE in the end?

If so, do you remember how difficult it was?

Cheers!

Cris