Interface and connectivity ICs

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Connect to TLV493D-A1B6 over I2C

Hi folksI am currently trying to communicate with the TLV493D-A1B6 3D hall sensor. As board, I'm using the NUCLEO-F103RB. To make sure I didn't mess up any connections or anything else, I verified my setup with an ADS1015 adc which I can read out ove...

Jiimmy by Associate II
  • 1874 Views
  • 5 replies
  • 0 kudos

STM32, SPI communication and SX1280.

Dear everyone,I'm trying to use a SX1280 for RF connectivity.My dev board is the official... the SEMTECH "SX1280ED1ZHP", it's included a nucleo + daughter board with SX1280.My diffculty is that a not able to read correctly a register with a know valu...

Capture d’écran 2024-11-28 143754.png Capture d’écran 2024-11-28 143319.png TEK0001.JPG TEK0002.JPG
JL_Loyd by Associate
  • 85 Views
  • 1 replies
  • 0 kudos

Resolved! S2-LP with Balun and RF Front-End

Hello,I am currently reviewing the S2-LP transceiver for high-bitrate/long-range communication in the 915MHz band. To achieve that, I want to interface an S2-LP with a Skyworks SE2435L front-end, as shown in the FK915V1 Evaluation board. I would like...

Chalumo by Associate
  • 492 Views
  • 3 replies
  • 1 kudos

S2-LP custom parameters

Hello, I'm evaluating the use of the evaluation kit and the evaluation software for the S2-LP to generate the OOK signal, In the software I can't modify the Preamble to a custom pattern, another thing is to be able to place the ID address (I can not ...

User2501_0-1730819906936.png User2501_0-1730804919129.png
User2501 by Associate II
  • 206 Views
  • 1 replies
  • 0 kudos

STPM3x Evaluation Board Shorting

 I am working with the STPM34/STPM33 chip and using the STPM34 evaluation board. I have noticed in my own hardware and the eval boards that when you attach power to measure voltage it shorts something and blows up. Is this a known issue? Is there a k...

IMG_2342 copy.jpg