Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST67W611M1 QConn_Flash failure

Dear all, I have designed a custom board using the STM32H563ZIT6 as the host MCU and the ST67W611M1 as the NCP. As part of the initial bring-up, I am attempting to flash the ST67W611M1 using the QConn_Flash_Cmd-ubuntu tool in standalone mode. For thi...

Multiplexing C/Q line with L6362A

Hi all,In order to have two possible functionalities on the same M12 plug I need to multiplex the C/Q line of IO Link with an analog input signal. The device is configured before the connection is established and it should stay in that mode during th...

JonasRitz_0-1776783858306.png JonasRitz_1-1776785075802.png

S2-LP AFC_CORR step size

The "S2-LP bring-up good practices v1.0.pdf" [1] document states the following information regarding AFC:"AFC_CORR is 2-complement byte (signed). Granularity is 508Hz for 50MHz Xtal"The mentioned step size of 508 Hz for a 50 MHz oscillator also corre...

emfend by Associate
  • 178 Views
  • 1 replies
  • 1 kudos

ST4SIM-200S Integration

Hi,1. can we interface directly ST4SIM-200S with LTE modem? 2. how we will integrate service provider like airtel/jio please share me any readable document that how it works with cellular network. 

kk1010 by Associate
  • 102 Views
  • 0 replies
  • 0 kudos

Resolved! ST67W61M1 Connection Errors and DTIM Issue

Hi,I am currently working on a feasibility project using the X-NUCLEO-67W61M1 and NUCLEO-U575ZI-Q.The sample code I am using is ST67W6X_FOTA.The FOTA functionality is working properly. However, during the initial connection phase, there is about a 50...

Jerrylin00_0-1776060565581.png