Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

NUCLEO-L476RG/IDB04A1 ITM and SPI

Posted on December 14, 2015 at 12:01Hello,I use a IDB04A1 bluetooth shield on a STM32L476RG Nucleo board and I want to redirect the standard output through the ITM port to see my printf in Keil uVision.The problem is that the SWOTRACE pin of the ITM...

vanson by Associate
  • 1066 Views
  • 0 replies
  • 0 kudos

Access point signal strength

Posted on December 10, 2015 at 13:40Dear STM, I would like to know if there is a command to get the RSSI of the AP which I am connected to. It seems that the only way is to perform a scan for all BSS. Thank you Paolo

paolo23 by Associate II
  • 848 Views
  • 1 replies
  • 0 kudos

socket server and multiple clients

Posted on December 09, 2015 at 17:53In my application, the SPWF01 needs to be both MiniAP and socket server.  I'm unclear how multiple socket clients would be supported - my understanding is that when in socket server mode, the SPWF01 switches to da...

bill by Associate
  • 932 Views
  • 1 replies
  • 0 kudos

Bringing up the BlueNRG device is failing!

Posted on December 01, 2015 at 10:53I am using BlueNRG ver 2 device, I'm using not an ST MCU, but freescale's.SPI was porting to my MCU Kinetis and the issue is:Instead of getting the ''Blue_Initialized_Event'' (0x04, 0xff, 0x03, 0x01, 0x00, 0x01), ...

0690X00000604wwQAA.png
guy by Associate
  • 1740 Views
  • 2 replies
  • 0 kudos

Brownout Event Problem

Posted on December 07, 2015 at 19:00Hi, I use Spirit1 both with 433Mhz and 868Mhz on the same custom-designed board with stm32l1. The radio parameters are set according to the individual transceiver and the software configuration is done seperately ...

hacer by Associate II
  • 1012 Views
  • 0 replies
  • 0 kudos

Error in X-NUCLEO-IDB04A BOM ?

Posted on December 03, 2015 at 23:18Hi, In this device BOM, L4 is listed as a ''tuning cap'' and value is 1.8pF which obviously does not sound like an inductor value... Seems to be the same with L2 which value is 0Ohm. Please, can anybody provide th...

JulienD by Senior
  • 711 Views
  • 0 replies
  • 0 kudos

SPWF01SC.21 module AT-commands library

Posted on September 25, 2015 at 13:41Hi, Is there any reference AT-commands library written in C for SPWF01 modules? Googling didn't help. Target OS is FreeRTOS, but generic C library is acceptable. I know, I can write it using state machines etc. I...

Grigori by Associate II
  • 4328 Views
  • 13 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.