STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How to unlock STM32H5 Flash?

I set my flash OB to iROT-Provisioned (Dont know exactly Product life cycle state, but I can not debug anymore) Based on my understanding, it may be in a CLOSED state. However, I am not sure how to change the state as I want to follow the Debug authe...

HNguy.27 by Associate II
  • 4460 Views
  • 6 replies
  • 0 kudos

TF-M and SBSFU Implementation on STM32U5A5

Hi @ChannelWe are using STM32U585 for implementation of TF-M and TF-M SBSFU for our project. now we are planning to change our controller to STM32U5A5 controller. I have couple of doubtsSTM32U585 is PSA Level3 certified while STM32U5A5 is not PSA lev...

PJose.4 by Senior
  • 1787 Views
  • 3 replies
  • 0 kudos

SBSFU on NUCLEO L452-RE

Hi,I am trying to implement SBSFU on NUCLEO L452RE board just by copying the project for NUCLEO L432KC (2_images, Y modem protocol) and changing necessary elements (target device, startup_***.s file, UART and led setup). When trying to download UserA...

ALazo.1 by Associate
  • 1503 Views
  • 1 replies
  • 0 kudos

Resolved! Passwords for RDP1 and RDP2

Hi there. Before attempting any password locking on my STM32575, I read the password lock location and it returned all zeroes like soReading 32-bit memory content Size     : 4 Bytes Address:   : 0x400220200x40022020 : 00000000After setting the PW, it...

PChoq.780 by Associate II
  • 2535 Views
  • 3 replies
  • 0 kudos

Resolved! SBSFU: Issue with 16-byte alignment in linker script?

I've run into an issue with the section of the UserApp linker script which ensures that the binary size is a multiple of 16 bytes:.align16 : { . = . + 1; /* _edata=. is aligned on 8 bytes so could be aligned on 16 bytes: add 1 byte gap */ ...

crwper by Senior
  • 3966 Views
  • 5 replies
  • 0 kudos

Unable to erase STM32H743 device. How to recover the device?

I have flashed the SBSFU application with write protection enabled for flash address 0x08000000. After that, I am unable to erase using jlink commander.exe as well as by IAR->project->Download->erase.STM32H743 has SWD interface and i am using jlink ...

0693W00000aJZHnQAO.png
mr.1 by Associate III
  • 3431 Views
  • 5 replies
  • 0 kudos

Resolved! Unable to execute my own application without TrustZone on STM32U5 (B-U585I-IOT02A) after executing SBSFU application example

Hi,I ran the SBSFU example of STM32CubeU5 following what is in the readme file without any problem. Then I disabled TrustZone but I cannot run the projects made with STM32CubeIDE, verification of the downloaded firmware fails. If I try to erase the f...

Domenico by Associate III
  • 3077 Views
  • 5 replies
  • 0 kudos