2022-05-04 11:38 PM
Hi ,
I am working on STM32U575 nucleo board .
Flash got locked (code freeze) and i have to power cycle board to run my application in below cases :
I am using 5V_USC_C to provide power supply to board.
Is this behavior acceptable , as going through some reference i have read that in RDP1 access via JTAG is considered as Intrusion and it locks Flash.
Does it applies to RDP2 also ?
@TDK @JHOUD
2022-05-05 9:22 AM
I don't know specifically about the STM32U5 series, but in other series (F4, L4, G4, F7):
Item 2 - yes, in RDP1 *OR* RDP2, any attempt to connect via JTAG or SWD will halt the CPU.
Item 1 - Don't recall if this is normal (needing power cycle after firmware activates RDP2), but it wouldn't surprise me if that was the case.
2022-05-10 11:54 PM
Hi @vsing.1 ,
first point - usually for the change in OB to become active the system needs to reload the OB. If you need power on reset to do OBL, then there is some problem in OBL_LAUNCH. But difficult to diagnose remotely, but check that.
second point - Bob answered correctly.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.