STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to chose random seed for RSA encrypt in X-CUBE-CRYPTOLIB?

The call to "cmox_rsa_pkcs1v15_encrypt" requires a "Random buffer" and a "Random Length (in Bytes)" as input parameters. It will return error code CMOX_RSA_ERR_WRONG_RANDOM if "Random material too short or not valid for the functionality".I keep gett...

LWChris by Associate III
  • 5733 Views
  • 13 replies
  • 0 kudos

Resolved! SBSFU --> MCU Boot with STM32U585 without Trustzone

Hi all,we would implement SBSFU (Secure Boot and Secure Firmware Update) on STM32U585.Our goals are:application do not use TrustZone feature (TZ_EN = 0)we want to avoid access to MCU on field (Device protection, for exapmle RDP = 1)question: if on fi...

SafeDev by Associate II
  • 3605 Views
  • 3 replies
  • 0 kudos

Resolved! SBSFU | KMS | How to use KMS_GenerateKeyPair()

Hello all.I have a question about how to use KMS_GenerateKeyPair() function. There are no examples in the code, and API description is not really enough for my little brain. Could somebody provide me an example on how it should be used? What kind of ...

SBSFU project structure and setup?

Hi,My question is about project structure.To implement SBSFU what is the best or correct approach if I have a project that I would like to flash to a target incorporating SBSFU?Import four project folders (SBSFU, SECoreBin, UserApp and MyProject) int...

DHard.2 by Associate II
  • 13789 Views
  • 9 replies
  • 0 kudos

Resolved! RDP of STM32G0B1xB/xC/xE

Hello .According to the reference manual, the default RDP level is set to level 1. However, after performing a full erase with ST-Link and then writing the hex file, the RDP level was found to be set to 0.I would like to set the RDP level to 1 at the...

aki49 by Associate II
  • 2742 Views
  • 4 replies
  • 2 kudos

Resolved! Regenerating OEMiRoT_Data.obk

Hi,While using the STM32Cube_FW_H5_V1.1.1 repository to explore secure boot on the STM32H5, I saw that the configuration file to generate OEMiRoT_Data.obk is missing. As I want to use my own keys and certificates for the OEMiRoT example application, ...

jens-vdb by Associate II
  • 3133 Views
  • 4 replies
  • 3 kudos

Resolved! BOOT_LOCK not cleared?

Hello,RM0444.Rev5 page 98 says that it is possible to reset it only when:• RDP is set to Level 0, or• RDP is set to Level 1, while Level 0 is requested and a full mass-erase is performed.I supposed that if RDP is changed from level1 to level0 then th...

S-.1 by Associate II
  • 1437 Views
  • 1 replies
  • 1 kudos