STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SBSFU - writing to MODER stops UART

Hi There,               I am trying to get our product working using the SBSFU on our product.  The latest problem I have is that the UART works when the application runs standalone - i.e. our code within the user app using the ST link, however, when...

Resolved! IOTA L2Sec stream fails due to STSAFE setup error

Hello,I'm trying to run the X-CUBE-IOTA1 v3.0 on the B-U585I-IOT02A board, but after following the tutorial in UM2606 I get the following error when trying to send L2Sec Stream:What can be the reason of the pairing_stsafe result failing, please?Best ...

SedCore_0-1707329532392.png
SedCore by Associate III
  • 4733 Views
  • 9 replies
  • 2 kudos

Example using STSAFE with Azue IoT

Hi,I'd like to ask if any example code for Azure IoT Hub group enrollment is available.I found examples for individual enrollment in X-CUBE-AZURE-v2-3-0 only.I try to follow the Just-in-time registration method and it fails when trying to connect to ...

neocnx by Associate
  • 2572 Views
  • 4 replies
  • 0 kudos

SBSFU - FW too big

I am adapting the NUCLEO-H753ZI single-slot project to work on a NUCLEO-H745ZI-Q board.My development environment is linux and I am using minicom for the ymodem upload.When flashed, the binary seems to function perfectly, but when I corrupt the image...

0693W000008y0DMQAY.png 0693W000008y0DRQAY.png 0693W000008y0DvQAI.png
AKhri.1 by Associate II
  • 2793 Views
  • 3 replies
  • 0 kudos

Port KMS to STM32H7A3

Hi experts,I need to implement the storage of a security key (upgradable) on STM32H7A3. After reading the example code of KMS under project B-L475E-IOT01A in x-cube-sbsfu, and a few posts in the forum (KSM support on STMH7  and 2-images-kms-port-to-s...

JQiao.1 by Associate II
  • 1380 Views
  • 1 replies
  • 0 kudos

Resolved! AES peripheral works differently

I want to use AES peripheral for encryption in ECB mode (256). I am able to encrypt and decrypt on the same MCU, but if I compare the encryption results, the HW peripheral has a different result than the SW library AES.c or encryption in Python - the...

JR2963 by Senior II
  • 4337 Views
  • 8 replies
  • 2 kudos

Resolved! Cryptographic Library

Hi,I am currently using the M3_CryptoFW_RngHW_2_0_6.lib for MDK-ARM. However, I must adhere to this specific library version, and I now need it for IAR, meaning that the required library is M3_CryptoFW_RngHW_2_0_6.a. How can I obtain this version for...

ari_v2 by Senior
  • 1908 Views
  • 2 replies
  • 0 kudos

Resolved! Updating the uROT signature remotely in a production device

Here is my attempt at background as I understand it... iROT is a ROM program in the STM32H563. It contains a P256 EC algorithm, and checks some section of FLASH that you define as a program for a signature, then jumps to it. The definition of the pro...

MBC by Associate III
  • 6287 Views
  • 6 replies
  • 2 kudos

Add a binary header and a sbsfu segment to an elf file

I have a problem with merge SBSFU .elf file and application .elf.I prepared:SBSFU.elf - addresses in linker script: 0x08000000 - 0x08020000application.elf - 0x08020400 - 0x081FFFFFheader.bin - size: 1024BSo I suppose, that like in SBSFU example heade...

MButk.1 by Associate
  • 4757 Views
  • 8 replies
  • 1 kudos