STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SBSFU File Missing error bin file of SECoreBin in STM32F769I MCU

 Hi all,I am using STM32F769I DISCO Board, STM32 CUBEIDE,X-CUBE-SBSFU 2.6.2 , WINDOWS Environment for checking new features in security i.e. secure bootloader.I am newbie to this topic and I have followed compilation procedure as per the readme file,...

lavanya by Associate III
  • 2336 Views
  • 1 replies
  • 1 kudos

Resolved! RDP level2 isn't compatible with WRP

Hello,please I need a confirmation about RDP level2 and WRP combination on stm32g031 chip.Based on RM0444.Rev5 Table 19, if I use my own bootloader and I write-protect the flash sectors, I have to avoid activating RDP level2 or I'll loose the opportu...

S-.1 by Associate II
  • 3533 Views
  • 4 replies
  • 3 kudos

Resetting an STM32H755 with secure area

I am building a secure bootloader on the STM32H755, but I've bricked a couple of boards now trying to get the secure areas working.I intended to use a "recovery" function on a button press to do a mass erase with protection removal. Then I can test e...

gpeh by Associate III
  • 8323 Views
  • 19 replies
  • 8 kudos

Resolved! configuration of the Tamper pins

Hi all,One small doubt on the tamper configuration, is it possible to configure both active and Passive tamper in the Same project/API, or  both should be in different project/API. why this doubt is as Seed is not required for Passive tamper, so does...

meghasb by Senior
  • 3528 Views
  • 5 replies
  • 0 kudos

TPM maximum NV storage size

Hello As in the title, for my project I'd like to know exactly what is the maximum storage capability/size of the device NV memory.The TPM used is ST33TPHF2XI2C.I wasn't able to find anything in ST documentation (datasheet, application notes).Waiting...

edopeter by Associate
  • 1808 Views
  • 1 replies
  • 0 kudos

AES in STM32F423

Hello  for allIn last days i was begin to implementation AES to work on stm32f423I am using example in NIST Special Publication 800-38A to take key-128 bit, input data that plain text , encryption and decryption data.but nothing seems to work , when ...

mick by Associate II
  • 1761 Views
  • 2 replies
  • 0 kudos

Resolved! How to integrate SBSFU in STM32U585 series

Hello support team,Have a Nice day.I am working on STM32U585ZIT6 Controller and investigating SBSFU for firmware upgrading.I list our specifications for a custom bootloader below.Enable TrustZoneEnable Dual bankRun time firmware write in the second b...

Secure key storage using SAES engine

Hi, with MCU STM32U585QII6QTR we encrypted an AES key using SAES engine and stored it in Internal Flash in RDP Level 0 and then moved to RDP Level 1. When we decrypt the key that was encrypted in RDP Level 0 using SAES engine, we didn't get our origi...

Kishore2 by Associate
  • 1424 Views
  • 1 replies
  • 1 kudos