STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Dynamic use of WRP (in STM32WBx5) ?

To secure my bootloader against erroneous writes from the application I want to enable write protection on it. But since for some things the bootloader needs to modify data inside its partition (security counter update and key invalidation), I can no...

OliM by Senior II
  • 3716 Views
  • 8 replies
  • 0 kudos

Resolved! SBSFU versus TFM for STM32U5G9J-DK2

# Overview I am looking into secure bootloader options for the STM32U5G9J-DK2 that support application updates. For now, I just wanted to run a demo that showed updating the application over UART.Initially I thought to start with SBSFU since that is ...

ttnickb_2-1731430416736.png ttnickb_1-1731430297792.png
ttnickb by Associate III
  • 3297 Views
  • 4 replies
  • 0 kudos

Resolved! Issue with STM32H735 Bootloader in RDP Level 1 (0xBB) Mode

Hello,I’m working with the STM32H735, and I need to enter bootloader mode to program the microcontroller. I modify the SYSCFG->UR2 register to set the address to 0x1FF00000, then perform a software reset. I use this method because I have no control o...

SHm by Associate II
  • 7776 Views
  • 12 replies
  • 1 kudos

Resolved! Secure Manager in DFU Mode

Hello, Actually am using STM32H5 board am able to load the secure manager using ST-Link Debugger but i would like to load the secure manager using usb dfu mode, is there any possiblity to load it.

Hitesh by Associate III
  • 5619 Views
  • 10 replies
  • 4 kudos

Resolved! OEM1KEY unlock sequence STM32U575

Hi,I am working on regression from RDP1 to RDP0 with OEM1KEY but made from inside and not by external debugger.I want  device to be able to make self unlocking.As I read in documentation RM0456, OEM1KEY unlock sequence requires:Shift OEM1KEY[31:0] th...

Pawel250 by Associate II
  • 1453 Views
  • 2 replies
  • 0 kudos

Non-encrypted binary can't be flashed properly

Hi everybody,I am using a platform that is based on STM32. The developers of this platform have provided to me the firmware image as an encrypted .bin file. When I flash it via USB everything is fine.Then I change their code and recompile everything ...

Lyap94 by Associate III
  • 1421 Views
  • 2 replies
  • 0 kudos

Resolved! ExitSecureMemory MPU region limitation (OEMiRoT)

The OEMiRoT project uses ExitSecureMemory V1.1 to enable 1 MPU region and start the application. This automatically enables the configured HDP region, so application cannot access the bootloader. The default OEMiRoT project allows for 2 tiny 64kB app...

Hans_W by Associate III
  • 2007 Views
  • 4 replies
  • 0 kudos