Security Workshop November 10th
I have not received the confirmation link and also not received the participation link. Please send me the participation link.
Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.
I have not received the confirmation link and also not received the participation link. Please send me the participation link.
Customizing the Cloud application from the STM32CubeExpansion_Cloud_AWS_V1.4.1causes the following link errors, where line 1 is the CubeIde generated linker command:I haven't change anything in the configuration. Just added codeAttached is the linke...
Greetings,Since I am on Linux and still wanted to do the hands-on parts of the workshop and the homework, I rewrote the provided Windows batch files as shell scripts. Couldn't really test all of them, but they're straightforward enough, and at least ...
In an Project, I'm using Jump to boot Function to jump to STM32 Factory Bootloader, so that i can able to load new firmware from USB via “STM32 Cube Programmer�? CLI Method (from our own system application).It is working fine when Read Out Protection...
Hi!I'm talking here about script "StartTTPL4.bat".I've removed "rem" before "pause" word at the end to see results of the script.Results are: "Error! No Com port available !"But I'm sute that it's available, because I can select it manually in terate...
I need to receive SPI data from STM32G474RE master A to STM32G474RE slave B with DMA and CRC feature. DMA works in normal mode both on master and slave, which triggered by timer 2 on master A. The structure of the data frame is ADC1(16bit)+ADC2(16bit...
I applied for 4th November session. To my knowledge, there was still no package received from ST to my address. Can you please confirm the shipment.Tnx & All the best, Mile
When it does not open any window, as it is mentioned in TFM_Homework.pdf, what can I do instead to know the board (STM32L5) is ready for "STM32 Security Workshop PSA-TFM"?I didn't see the windows in the attachments.
Hi, I have used STM32H750VB IC and have done SHA256 conversion of a given data using an inbuilt functionHAL_HASHEx_SHA256_Start(&hhash,(uint8_t*)'A',sizeof('A'),(uint8_t*)aSHA256Digest,200);HAL_HASHEx_SHA256_Finish(&hhash,(uint8_t*)aSH...