STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H743I6-EVAL2 USB HID not working

Hi,I load a basic HID program in ST Cube IDE which is working perfectly on NUCLEO-H743ZI2With the eval board, when i plug CN18 USB to my PC it says "Unknown USB Device (Device Descriptor Request Failed)"I can't find where it is coming from, any ideas...

STM32Cube project for Ethernet examples

I would love to get my hands on a STM32Cube project for the STM32F4xx_Ethernet_Example\Project\FreeRTOS\httpserver_socketI would like to make a webserver on the demo board, but don't know how to set up the STM32F407 MCU in the Cube.The demo's are gre...

PJera.1 by Associate II
  • 625 Views
  • 0 replies
  • 0 kudos

STM32F407 VCP Freertos recive data problem

I'm trying to make a vcp implementation with STM32f407 and freertos.I have no problem sending data from STM to my pc.When I send data from PC to STM, when I send a few tens of bytes of data, the CDC_Receive_FS function is triggered several times and ...

Resolved! STM32F4 Use HSI for USB Clock

I want to use STM32F413 for my PCB design. I need USB data lines for communicating with a computer. Ideally, I would not have any oscillator on the PCB to save space. I noticed that's it's not possible to use HSI for the USB clock on CubeMX. Can I us...

0693W0000059C4mQAE.png 0693W0000059C56QAE.png 0693W0000059C5LQAU.png 0693W0000059C5QQAU.png
JBret.1 by Associate II
  • 10525 Views
  • 12 replies
  • 0 kudos

What's wrong with the compare in STM32F373?

I use MDK 5.32. In the debug interface - Peripherals - System Viewer - COMP window, the value of CSR is always 0 after initialization and the address of CSR is viewed as 0x40007C1C. But CSR's address is 0x4001001C in STM32F37xc.h. What's the mat...

0693W000004JKJRQA4.jpg
yundm2 by Associate II
  • 1333 Views
  • 1 replies
  • 1 kudos

GOOSE message sending using lwip

I'm trying realize with IEC61850 . I try to do GOOSE Publisher device. As I understood, GOOSE message goes to NET without any headers. I use lwip library. I found there IP_Forward functions, wich help send dirrectly my message to NET. But it also add...

0693W00000597ziQAA.jpg
ASemy.1 by Associate
  • 2455 Views
  • 1 replies
  • 0 kudos