STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 Functional Safety

This follow up question of STM Functional Safety webinar. It was not clear from the webinar if drivers and device specific CMSIS code generated by STM32Cube is certified for functional safety standards?

How to check that my hostname is stored in DNS server

Hello,I am working with an STM32F4. My goal is to be able to access to the board using its hostname. From what I've seen, to get it done I have to :    set LWIP_NETIF_HOSTNAME to 1   set LWIP_DHCP to 1I also set LWIP_DNS to 1.I made few modification ...

0693W00000JMU5zQAH.png 0693W00000JMU4SQAX.png 0693W00000JMU5RQAX.png
Aahai.1 by Associate
  • 1499 Views
  • 0 replies
  • 0 kudos

Hello, I try to implement a dual cdc with two virtual port com on USB_FS and HS. Receives callbacks works well on both VCP but only transmit on the first VCP works. When I try to send data from the STM32 to the second VCP, nothing append.

OTG_FS_IRQHandler is endlessly called"signal handler called>() at 0xffffffe9"I have already increase the heap and stack size to 0x2000. I use the STM32H753i-EVAL2 board

JHAPP.1 by Associate II
  • 1806 Views
  • 3 replies
  • 0 kudos

Resolved! USB CDC (or whatever else): how do I rename my device?

Hello!Almost everything is in the title. Is there a way to rename the device I'm developing.When I lsusb, it says STMicroelectronics virtual COM port. How do I change that toMyDeviceName?Beside this, is there a need to get a vendor ID / product ID? I...

PG.1 by Associate III
  • 1654 Views
  • 1 replies
  • 0 kudos

Resolved! How to delete local host keys in ST-SAFE-A110?

Hi.Im working with ST-SAFE-A110 together with STM32CubeExpansion_STSAFE-A_V1.2.0 in a STM32_L4.Im trying to change my local host keys after being populated. I can wrap/unwarp without any problems but I don't know how to erase and regenerate the keys....

PLori.1 by Associate
  • 1637 Views
  • 1 replies
  • 0 kudos

STM32H757 - Start up issue and sync

I am working with the STM32H757 on a custom board.The M7 runs with FreeRTOS, the M4 is bare metal. Both cores have output GPIOs connecteed to LEDs which allow me to make sure that both of the cores are up and running.At the begining of the code for ...

yuri CH by Senior
  • 1488 Views
  • 1 replies
  • 0 kudos

MQTT broker running on STM32F7

Hi everyone,I need to run a MQTT broker on my board powered by a STM32F746. I managed to get the LwIP stack running properly as a starting point. I verified this by sending and receiving topics with the provided MQTT client implementation of LwIP.LwI...

CA_SUS by Associate II
  • 2595 Views
  • 2 replies
  • 0 kudos

Use UART DMA with X-CUBE-CELLULAR

Hi everyone,​I am using X-CUBE-CELLULAR v6.0 and would like to use DMA on UART to replace the original interrupt receiving method. ​The original method is calling IPC_RXFIFO_writeCharacter() in HAL_UART_RxCpltCallback() and notify upper layer when an...

SL61 by Associate II
  • 716 Views
  • 0 replies
  • 0 kudos