STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! HAL SPI library: Does Master's single call to HAL_SPI_Transmit() always trigger Slave's both HAL_SPI_RxCpltCallback() and also HAL_SPI_TxCpltCallback() ?

I am coding STM32H743 MCU with CubeMX generated library.I have 1 SPI Master and 1 Slave. Both configured for a full SPI with both lines of Tx and Rx.Master is calling blocking HAL_SPI_Transmit() or HAL_SPI_Receive() but never simultaneous HAL_SPI_Tra...

eBirdman by Senior II
  • 2871 Views
  • 3 replies
  • 0 kudos

Writing own drivers vs HAL for professional project

Hi,firstly i apologise if this is in the wrong section as I'm asking more for technical advice than an answer for a specific technical question.First a bit of background:I'm a PhD student that is the sole engineer on a three year project that include...

CDyer.1 by Senior
  • 10927 Views
  • 28 replies
  • 4 kudos

How can I add "next_tag_part" to my function?

My string is too long to be inserted at once! And according LWIP manuals:LWIP_HTTPD_SSI_MULTIPART==1: SSI handler function is called with 2 more arguments indicating a counter for insert string that are too long to be inserted at once: the SSI handle...

DK.7 by Senior
  • 948 Views
  • 0 replies
  • 0 kudos

Resolved! STM32G0B0: Prevent bootloader execution after RDP regression from level 1 to 0 and OBL causing mass erase and system reset

Hello,I would like to know how to prevent the execution of the on chip bootloader after a RDP regression from level 1 to level 0. After the necessary option byte load (OBL) a mass erase is done and the chip is reset and after the reset the bootloader...

DaMCU by Associate II
  • 4843 Views
  • 9 replies
  • 0 kudos

Resolved! is STM32F7 has DFSR register?

Hi!I try to understand debug information after hard fault. RTOS dump DFSR register (and some other) after fault to UART. This register is not present in PM0253 programming manual, but there is definition in source code (core_cm7.h address is 0xE000ED...

Aleks by Associate III
  • 1512 Views
  • 3 replies
  • 2 kudos

Resolved! Does the DMA Arbiter allow round robin preemption after each piece of data to keep multiple peripherals going at once or does the DMA controller completely block until an entire block of data has finished transmitting?

I am working with the STM32L4S9AII6 MCU on a project where I am being asked to replace an FPGA implementation with this CPU. We are maxing out all 14 DMA streams via SPIs, I2Cs, & UART. As you can imagine, I am working with some serious hard real-tim...

MFolk.1 by Senior
  • 1631 Views
  • 2 replies
  • 0 kudos