STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Nucleo-F411RE uart bootloader don’t work.

I am developing with Nucleo-F411RE Board an trying to use UART2 bootloader to flash my program.I use STM32CubeProgrammer to do this.when connect my board, ide report that Error: Activating device: KO. Please, verify the boot mode configuration and ch...

0693W00000SvJs3QAF.jpg 0693W00000SvJswQAF.png

How can I synchronize a timer to USB SOF?

I'm interested in trying to synchronize my system to USB start of frame packets. I'm using the CRS system to generate an HSI48 clock. I've considered running that HSI48 clock into MCO and using that as an external clock for a timer. This would enable...

Lee3 by Associate III
  • 1662 Views
  • 1 replies
  • 0 kudos

There is an error in AN3155 Rev 15 page 26/48, Figure 15. After the first ACK you send either a special command that starts with 0xFFFy or the number of pages to be erased.

This is supported by the previous page Figure 16. The ACK is sent then if it is a special erase you send it the 2 bytes special code. If it is not then you send the number of bytes for the number of pages you want to erase, then the pages to erase, t...

KiptonM by Lead
  • 1551 Views
  • 2 replies
  • 0 kudos

Resolved! Run ThreadX on Windows

Hey threre,I am thinking about to switch from freeRTOS to ThreadX on STM32H7. But there is a important question. Is it possible to run ThreadX on Windows? We want to simulate some parts of our firmware. I know that there is a port for WIN32 and there...

ESawa.1 by Senior
  • 5506 Views
  • 6 replies
  • 0 kudos