STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Ethernet MAC Filtering

Good morning friends,Now I receive multicast on STM32F437, it works. But I would like to add filtering. And I have a problem with that.IGMP and others, I have it enabled.Now my settings.macinit.MulticastFramesFilter = ETH_MULTICASTFRAMESFILTER_PERFEC...

F411 I2C LL Call Hangs

I am using F411 to communicate with ADXL355 through I2C1.I have a very strange issue: LL_I2C_GenerateStartCondition(I2C1); /* (1.3) Loop until Start Bit transmitted (SB flag raised) ********************/ /* Loop until SB flag is raised */ w...

HDaji.1 by Senior
  • 2311 Views
  • 3 replies
  • 0 kudos

Problem with USB composite device on STM32H750

Composite device: Microphone+ Speaker+ MSC+ Hid Keyboard+ Hid Mouse.Windows sees it in the device manager.The packages from the Hid Mouse pass and the cursor moves.Packets from the HID keyboard pass (visible in USBlyzer), but the keystrokes are not d...

TDerk.1 by Associate
  • 1349 Views
  • 1 replies
  • 0 kudos

STOP2 mode and FreeRTOS

HiI want to use FreeRTOS with low power STOP2 mode without using the ticklessidle mode.One of the tasks once every cycle goes sets the mcu into stop2 mode.I’m using both RTC and LPUART for waking up the mcu.when using with just two FreeRTOS tasks all...

deckhard by Associate III
  • 1248 Views
  • 1 replies
  • 0 kudos

Do I need to configure USB FS with the STM32CubeMX tool in the STM32CubeIDE for the built-in DFU bootloader to work?

I am using the STM32G474RE and according to AN2606 Rev 55, it has a built-in bootloader in system memory. I set the option bytes such that the MCU boots from system memory and I will use the STM32Cubeprorammer CLI to program via USB. In my applicatio...

JZepe.1 by Associate
  • 1136 Views
  • 1 replies
  • 0 kudos

Transmit data through CDC VCP Failed error

I am trying transmit data using CDC(virtual port) in NUCLEO-H743Zi2, but I am getting this error when I plug in my VCP port to my pc (Unknown USB Device (Device Descriptor Request Failed)), I could not find a way to fix it.My hardware settings:MCU sp...

AElta.1 by Associate II
  • 2329 Views
  • 5 replies
  • 0 kudos