STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! About GPIO

I am using a nucleo l4r5zi.​I would like to use the GPIOs on this board as inputs and get the value of those inputs from software.Specifically, I would like to use PG2 to accomplish this.​I have the following setup and am inputting 3.3v into PG2, but...

Myasu.1 by Senior
  • 4114 Views
  • 6 replies
  • 0 kudos

STM32F767ZI + FreeRTOS SysTick HardFault

Hey! I'm not that experienced wit FreeRtos and i am facing a HardFault problem. I want to use FreeRtos and created some tasks. But when the Systick Handler is called for the first time, it causes an Hardfaul Exeption. The Program Counter points to th...

MKuhl.1 by Associate II
  • 4380 Views
  • 5 replies
  • 0 kudos

Problem using ethernet connection in Nucleo-h743zi2

hi I am using Nucleo-H743ZI2 for Ethernet :Ethernet RMII: First TxDescribter Address: 0x30000200.First RxDescribter Address: 0x30000000.Rx Buffers Length: 1536.CortexM7 setup:LWIP:key options:LAN : Platformadd to Flash.id: .lwip_sec (NOLOAD) : {  . =...

0693W00000UnbfTQAR.png 0693W00000UnbgCQAR.png 0693W00000UnbgHQAR.png 0693W00000UnbggQAB.png
AElta.1 by Associate II
  • 1734 Views
  • 1 replies
  • 0 kudos

Resolved! ULPI on the STM32H7B0 using USB3300

I had success when using the ULPI interface on a STM32H7A3 (on the nucleo board) using an external ULPI transceiver board https://www.waveshare.com/usb3300-usb-hs-board.htmbut when porting over to the STM32H7B0, I am not having much success. I believ...

Resolved! STM32 for safety critical application.

Hello, I happened to have to make an MCU board for a military application. Generally I always use STM32 MCU with which I am very comfortable.But for this specific application I tried to search if there were any MCUs specifically designed for mil...

LWIP: allocation fails in Heap (mem_malloc) for TX

Hello,I'm on a STM32H743 (nucleo-H743ZI2), and I got LWIP (no OS) to "work", as in it receives ip packets and reads them. The problem is with allocating on the heap. I didn't use the libc_malloc option, the heap pointer is at 0x30044000 and is 1600 b...

gdere.1 by Associate
  • 3240 Views
  • 2 replies
  • 0 kudos

Resolved! AUDIO_AudioCmd_FS gets called only once

I am trying to implement a simple soundcard from using STM32F407G-DISC1 board.It utilizes STM32F407. I am using CubeIDE version 1.10.1I configured the USB to be Full-speed Device Only. And I configured the middleware as Audio class.I set the the heap...

Sami1 by Associate II
  • 1632 Views
  • 1 replies
  • 0 kudos

HAL UART Receive short reads - corrupt data

I am trying to implement a UART Rx using a typicalstart-byte, length, payloadpattern.I spin read on 1 character until it is my start byte. Then I read 2 bytes, shift them into a 16 bit length and read the remainder of the payload.The trouble is, the...

PCamp.2 by Associate III
  • 3623 Views
  • 6 replies
  • 0 kudos