STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB Host on STM32F7 - Suspending a device

I am using the ST Host library version 3.54 on an STM32F769 device, supporting HID devices.  I am using the internal Full Speed phys.I have a USB mouse connected and all works fine, however I would like to save power when the mouse is not being used ...

barryccl by Associate II
  • 255 Views
  • 2 replies
  • 0 kudos

Nucleo-H753ZI USB Audio firmware examples

Hello, I wonder that examples could apply Nucleo-H753ZI board... There are some examples about H743 or another one but no example for Nucleo-H753ZI board.    I understand 48k-2channel-16bit can be implemented easily, But I wonder that Nucleo-H753ZI c...

skson by Associate II
  • 941 Views
  • 6 replies
  • 0 kudos

RTOS selection for STM32H7R/S

We are starting to develop a new hardware platform and are currently evaluating the STM32H7R/S series for the main controller.The question now is which RTOS is best suited here in terms of long-term support from ST. We're going to use a lot of commun...

tdecker2 by Associate III
  • 1334 Views
  • 7 replies
  • 4 kudos

STM32U5 USB Interrupt Based Approach

I am using the STM32U585RIT6 microcontroller with the B-U585I-IOT02A development kit. I need to implement USB functionality using an interrupt-based approach. In my project, I have configured USB_OTG_FS in Device-only mode, enabled the NVIC global in...