STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPI2 STM32H745

Hi everyone I can find help on how to connect SPI2 STM32H745. I have read the datasheet and did everything written on it.Please can someone help me 

fru999 by Associate III
  • 2700 Views
  • 4 replies
  • 0 kudos

Resolved! H5 1.2.0 and Cube 1.5 break ethernet

After updating Cube to v1.5 for my STM32H5 project (Nucleo-H563ZI), the ethernet stopped working except during the initial run after a load of the firmware with the debugger.  After a reset, either POR or via the debugger, pings to the board fail.  W...

robmilne by Associate III
  • 3557 Views
  • 5 replies
  • 0 kudos

Resolved! STM32H745 SPI Accelerometer ADXL355

Hi everyone, I am trying to use an accelerometer with my STM32h745 board thought SPI.DO you have any idea where I can find library for thus accelerometers ?And how to use the SPI protocole with STM32H745 :)

fru999 by Associate III
  • 1950 Views
  • 1 replies
  • 0 kudos

PHY ETH implementation

Hi, community!As I am dealing with STM32 at the first time, I need help. With my colleague we are doing our first project on STM32 (stm32F767ZITx). We need TCP/IP, so I've added to project FreeRTOS-PLUS. According to FreeRTOS-Plus-TCP Networking Tuto...

braboar by Associate
  • 1185 Views
  • 1 replies
  • 0 kudos

Resolved! Differnce between UART and RS232

Hello everyone, I'am designing a model rocket flight computer. This is a two stage rocket so that's mean I will use two flight computer.Flight computers should have a communication between themselfs. For this communication which one is better? Direct...

testbenchmark_0-1716662112256.png

Resolved! Is the ITTIA database free for the STM32?

Hi CommunityI'm working on a project with stm32F407VET6, and I need a database for storing data. I found the ITTIA DB, and I install it from stm32 cube ide in the middleware categories (FreeRTOS support) but when I read the documentation in the offic...

Resolved! STM32U575 VREFBUF Driver bug when 2.5V is set

Hello,Just fount a bug on the LL driver of VREFBUF on STM32U575when you want to configure internal Vref to 2.5V and you use the nest function:LL_VREFBUF_SetVoltageScaling(LL_VREFBUF_VOLTAGE_SCALE3);where LL_VREFBUF_VOLTAGE_SCALE3  should set VRS bits...

Daniel_A by Associate
  • 1608 Views
  • 1 replies
  • 2 kudos