STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to change the IP Address at runtime

This is my Environment:Microcontroller: STM32H723ZET6LWIP is used. No RTOS used.I am setting a Static IP address in the *.ioc file. I am setting the same IP address in the TCP Raw Socket Echo Server to Bind the socket. Over that I am running the Modb...

Resolved! Eeprom Emulation on STM32H723

Hello, i am trying to implement Eeprom Emulation on STM32H723 using the code that ST provided in STM32CubeH7-Master for STM32H743 series. In the EE_Init function, first thing that function does is this line of code:   PageStatus0 = (*(__IO uint16_t*)...

mazotcu16 by Associate II
  • 2133 Views
  • 2 replies
  • 3 kudos

HardFault inside System Init - STM32L151CBUxA

I am trying to run a code that's built using STM32L1x_Peripheral Libs for STM32L151CBUxA MCU.As soon as I run the SystemInit function inside the ResetHandler I am hitting a Hardfault, so I investigated the SystemInit function.Once the Vector Table re...

gkowshik_0-1727875652572.png
gkowshik by Associate II
  • 2986 Views
  • 6 replies
  • 1 kudos