STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Dual bank booting problem

Hello!I try to use dual bank option on the stm32l476 (256kB) for implementing a custom bootloader. I want just read new program (bin) by custom protocol and write it to another bank. After that I want to switch the banks, reset mcu and start the new ...

KKlyn.1 by Associate II
  • 2812 Views
  • 5 replies
  • 1 kudos

Unable to get the IP using DHCP

Hello everyone,   I am trying to get an IP for my controller using the DHCP i can able to detect the Link up and link down but i can't able to get the IP. I had refered the example code for the ethernet(lwip https server netconn rtos) But i can't abl...

HELP with Burst Mode HRTIM

  Hi everyone, I am working on an STM32G4 project using the HRTIM1 peripheral. My goal is to generate a burst of exactly 3 PWM pulses on Timer A and Timer B simultaneously, triggered by an External Event (Sync Input / EEV). The Goal: System waits fo...

NUCLEO-G0B1RE with SNK1M1 only DEFAULT 5V

Hi STM32 community, I have ordered those the Evalboards: NUCLEO-G0B1RE X-NUCLEO-SNK1M1 - USB Type-C Power Delivery Sink  I have followed all of your existing applications, but none of the had lead to an similar result as displayed by your application...

kuda1311 by Associate II
  • 504 Views
  • 3 replies
  • 0 kudos

no RTC wake up

I’m working on a project with the Nucleo-L476RG. I want to perform a measurement, then put the microcontroller into Sleep Mode for 2 seconds, after which it should be woken up by the RTC clock.I followed the tutorial:How to configure the RTC to wake ...

MichalPorazko_0-1764697557739.png MichalPorazko_1-1764697599975.png MichalPorazko_2-1764697651032.png MichalPorazko_3-1764698784445.png

Resolved! STM32N6 FreeRTOS linker issue for MPU

I am trying to setup FreeRTOS for the new STM32N6 Nucleo board. Running into the following error `GCC/ARM_CM55_NTZ/non_secure/port.c:1814: undefined reference to `__privileged_sram_start__'`.Based on https://github.com/STMicroelectronics/x-cube-freer...

milanvdm by Associate II
  • 1886 Views
  • 2 replies
  • 0 kudos