STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32C071 USB Host

I'm looking to implement USB host functionality on an STM32C071 to connect with a single device that sends/receives serial data over USB so the only class I'm interested in is CDC, but I'm having trouble using USBX (I'm not using RTOS). For now I hav...

usbh.png class.png usbx.png
vermas by Associate
  • 288 Views
  • 2 replies
  • 0 kudos

Levelx without Filex

Hi Everyone, I one of our project i want to store the logs on NOR flash. I want to use Levelx to take care of NOR flash low level . But as per documents levelx can be used with Filesx, Is there is any way that i can use Levelx with Filex?

Resolved! STM32 Write to internal EEPROM only work once

Hi people,i have trouble with writing to the internal eeprom / flash. I can write values one time to the EEPROM and read it correct back from eeprom. When i write next time values to the eeprom and read them, the values changed but are incorrect. I t...

Stefan-G by Associate II
  • 394 Views
  • 7 replies
  • 6 kudos