User Activity

Hello everyone,I am developing firmware for the STM32F7469I discovery board, and I'm utilizing TouchGFX for the GUI aspect of the project. However, I am encountering a problem when enabling USB-FS HOST functionality. The GUI and other peripherals suc...
Hello everyone,I am currently developing a GUI for the STM32F469I Discovery Board using the TouchGFX IDE. The GUI works perfectly when updated through the TouchGFX IDE.However, when I attempt to update the same project using STM32CubeIDE, I encounter...
we are working on a project where an STM32F4 microcontroller is used as a host to connect with an external device. we are considering using the USB interface for this purpose. Can we refer to the following example to implement USB host functionality ...
Kudos given to