STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ETH on STM32H743 with Zephyr

Dear,I'm trying to use the ETH with Zephyr RTOS 3.5.99. It was built the samples/net/dhcpv4_client sample, however, I tried to build others examples from samples/net/socket, such as echo and echo_client, but was impossible.I would appreciate it if an...

USART_WakeUpFromStop1 leads to lost characters

While experimenting[*] with the USART_WakeUpFromStop1 example on my NUCLEO-L496ZG I noticed that repeatedly entering STOP1 mode leads to dropped character if running with a baudrate > 4800 bps. I'm using STOP1 mode in a different project and I hoped ...

BErik.1 by Associate III
  • 3015 Views
  • 9 replies
  • 0 kudos

DMA Interrupt not trigger

here i generate pulse using pwm generation.. where i need to stop at n th pulse.. so i use RCR register to stop it..where my mcu handle only 8 bit data to the RCR register.. so i split the data into array "RCR_Data" and stores as source destinationi ...

RAM test method for X-CUBE-STL

Hi,I am reviewing the Safety Manual to utilize the Self-Test Library provided by ST, and I have questions about the RAM Test method.It is mentioned that STL provides RAM Test using the March C-algorithm, and its verified diagnostic coverage can satis...

yang90 by Associate
  • 3083 Views
  • 2 replies
  • 0 kudos

HAL_Delay() Not Working Before OS Kernel Start.

Hi,I need to initialize a display by calling my function in main.c. This function uses the I2C4 channel and requires implementing some delays.Since it uses I2C4, it must be placed after the CubeMX Init functions, specifically in /* USER CODE 2 */. Do...

Ricko by Senior III
  • 3821 Views
  • 5 replies
  • 1 kudos