STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! SPI STM32H743 function problem

Hi, I have problem with my SPI peripheral. For generate inicial code I used STM32 Cube IDE Version 6.14.1, and programming IDE STM32 Cube IDE Version 1.18.1.Description of problem:1.I want simple to check loop with transmit and receive data, but when...

HAL_PCD PCD_GET_EP_RX_CNT only return 0

Hello, I am working on a stm32u083rc. I'm trying to establish a USB Serial connection using the HAL_PCD library. I'm at the enumeration stage and trying to read the data sent by the PC (windows).The USB device is initialized with CubeMX (STM32Cube FW...

Resolved! HAL_DMA_RegisterCallback with SPI

Hi, I'm just struggling with the same problem. I use SPI with DMA non-circular mode and want a callback for receive complete. I can set the callback function with HAL_DMA_RegisterCallback but in HAL_SPI_TransmitReceive_DMA it will be overwritten: /*...

STmine by Associate
  • 1338 Views
  • 3 replies
  • 0 kudos

STM32N6 SystemIsolation_Config

 Hello all,I'm working with the STM32N6 series and I'm trying to correctly configure the isolation between the secure and non-secure domains using the RIF (Runtime Isolation Framework).I found example code like this in a template (STM32CubeN6)  stati...

Help with host USB Printer Class

Hi,I know this question have been asked many times but i still can find a solid answer that can really help.I will try to ask again depends on the progress i have made and i hope if someone made this class that he could help.My objective is to be abl...

H_Drx by Associate II
  • 2248 Views
  • 3 replies
  • 0 kudos

Resolved! LwIP Socket TCP Server communication problem

Dear STM32 Community,I'm currently working on a bare-metal project with the STM32H723VG using the LwIP stack. I've implemented a TCP Echo Server based on the examples provided in the STM32Cube repository.The application works as expected when I open ...

adakPal by Associate III
  • 2287 Views
  • 1 replies
  • 1 kudos