STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! xSemaphoreCreateBinay() crash IOs

IDE : STM32CubeIDE Version: 1.16.1Board : STM32F407VG DISC1SYS Timebase Source : TIM6 Hello,In my project, i use I2C and multiple UARTs. It worked fine before adding FreeRTOS tasks. Recently i need add buttons to my project, so i add a new task to ha...

STM32H723 PTP IEEE 1588V2 support

I am currently using STM32H723 MCU for a project. I want to use PTP to synchronise different peripherals that will send data and their timings need to be precisely synchronised. The reference manual has got a whole section for programming IEEE 1588 t...

Resolved! STM32 CDC ECM HOST Lib

Hello,I'm working on an adapter USB to Ethernet and it is working only as a DEVICE. Now I would like to do the same but I want my STM to work as HOST.Is ST providing the same code stm32-mw-usb-device but for host?Thanks,G.

Gwen1 by Associate III
  • 1782 Views
  • 3 replies
  • 1 kudos

How to test STM32CubeExpansion_STL_G0_V2.0.0

Dear ST,   After signing the NDA agreement, I received STM32CubeExpansion_STL_G0_V2.0.0.   I tried testing the projects for NUCLEO-G071RB in STM32CubeIDE 1.14.1, but to no avail. Edit: Removed screenshots as package is under NDA. After importing the ...

Kolkentu by Associate II
  • 900 Views
  • 4 replies
  • 0 kudos

Resolved! SPI slave mode - data losing

HelloI have two boards. Both of them are based on STM32 MCUs. One is a SPI master and the second is a SPI slave.Settings for master (STM32H723): mHandle.Init.Mode = SPI_MODE_MASTER; mHandle.Init.Direction ...

Oleksandr_0-1717081696365.png Oleksandr_2-1717082783119.png Oleksandr_3-1717083091971.png Oleksandr_5-1717083347815.png
Oleksandr by Associate III
  • 5236 Views
  • 9 replies
  • 3 kudos