STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

UART with DMA RX/TX

Dear ST's experts,I want to send/receive data through UART between STM32 and PC. The data must be sent to PC every 500ms and then STM32 receive data from PC. I have configured UART2 with DMA in circular mode. I am using the function HAL_UART_TxCpltCa...

Resolved! SPI with DMA failing on second pass

I'm looking for some guidance on using DMA with SPI. I have the M4 core on an STM32H755 set up as a master in full duplex mode, and as long as I invoke the SPI transfer using interrupts, the program runs fine. When I try to migrate to DMA, however, I...

VO by Associate III
  • 1008 Views
  • 2 replies
  • 1 kudos

Resolved! Stm32f407 FPU with threadX

Hello everyone,I'm using AZURERTOS on my STM32F407 microcontroller. My goal is to use the FPU to perform some mathematical operations (FFT, etc.). Could you help me figure out how to activate the FPU and how to tell when it's active, taking into acco...

STM32H523HEYX flash write issue

STM32H523HEYX Flash Write Issue1.I’m currently working on a project using the STM32H523HEYX.I'm using STM32CubeIDE, and the firmware libraries are up to date.I’m also using STM32 X-CUBE-FREERTOS.I’m trying to write data to Flash memory using the foll...

yb25Kim by Associate
  • 713 Views
  • 1 replies
  • 1 kudos

IAP problem?

Hello everyone,I ran into a problem. First of all, I have two tablets: one with a bootloader and another without it. Tablet without bootloader works fine so its something bad in bootloader. I’m trying to plug in and unplug the power supply, and somet...

heyo_0-1752824790197.png
heyo by Senior
  • 1149 Views
  • 5 replies
  • 0 kudos