2025-07-18 2:02 AM - edited 2025-07-18 4:30 AM
Hello.
I've been struggling for several weeks to fix an issue when sending data over MQTT using LwIP on an STM32F407 microcontroller.
For periodic message publishing, I'm using the following code:
void MqttPublishTask(void const * argument)
{
err_t err;
while(1)
{
xEventGroupWaitBits(mqttSendEventGroup,
pdFALSE,
pdTRUE,
portMAX_DELAY);
if(mqtt_client_is_connected(&client))
{
cJSON *root = cJSON_CreateObject();
for(uint8_t i = 0; i < (nodeID - 64); i++)
{
cJSON *tap_metrics = cJSON_CreateObject();
cJSON_AddNumberToObject(tap_metrics, "ER", taps[i].alarmCode);
cJSON_AddNumberToObject(tap_metrics, "C", taps[i].coldWater);
cJSON_AddNumberToObject(tap_metrics, "H", taps[i].hotWater);
cJSON_AddNumberToObject(tap_metrics, "E", taps[i].totalEnergy);
cJSON_AddNumberToObject(tap_metrics, "T", taps[i].waterFlowTime);
cJSON_AddNumberToObject(tap_metrics, "N", taps[i].numberOfUses);
snprintf(serialString, sizeof(serialString), "%lu", taps[i].serial);
cJSON_AddItemToObject(root, serialString, tap_metrics);
}
char *pub_payload = cJSON_PrintUnformatted(root);
uint8_t qos = 0;
uint8_t retain = 0;
snprintf(serialString, sizeof(serialString), "%lu", OD_PERSIST_COMM.x1018_identity.serialNumber);
err = mqtt_publish(&client, serialString, pub_payload, strlen(pub_payload), qos, retain, mqtt_pub_request_cb, 0);
if(err != ERR_OK)
{
printf("Publish err: %d\n", err);
}
cJSON_Delete(root);
free(pub_payload);
}
osDelay(30000);
}
}To establish and check the connection with the broker and also for debugging purposes, I’m using the following task:
void MqttConnectTask(void const *argument)
{
mbedtls_threading_set_alt( cmsis_os_mutex_init,
cmsis_os_mutex_free,
cmsis_os_mutex_lock,
cmsis_os_mutex_unlock );
if (tls_config == NULL)
{
tls_config = altcp_tls_create_config_client(
(const unsigned char *)mbedtls_root_certificate,
sizeof(mbedtls_root_certificate));
if (tls_config == NULL)
{
printf("Failed to create TLS config\n");
vTaskSuspend(NULL);
}
}
ip_addr_t mqtt_server_ip;
while (netconn_gethostbyname("my.mqtt.broker.es", &mqtt_server_ip) != ERR_OK)
{
printf("MQTT Server DNS resolve failed\n");
osDelay(5000);
}
memset(&ci, 0, sizeof(ci));
snprintf(serialString, sizeof(serialString), "%ldc", OD_PERSIST_COMM.x1018_identity.serialNumber);
ci.client_id = serialString;
ci.client_user = "username";
ci.client_pass = "password";
ci.keep_alive = 14;
ci.tls_config = tls_config;
while (1)
{
if (!mqtt_client_is_connected(&client) && netif_is_link_up(&gnetif))
{
xEventGroupClearBits(mqttSendEventGroup, MQTT_SEND_EVENT_RUN_BIT);
mqtt_disconnect(&client);
if (client.conn != NULL)
{
altcp_abort(client.conn);
client.conn = NULL;
}
memset(&client, 0, sizeof(client));
osDelay (100);
printf("Attempting MQTT connect...\n");
err_t err = mqtt_client_connect(&client, &mqtt_server_ip, 8883, mqtt_connection_cb, 0, &ci);
if (err != ERR_OK)
{
printf("mqtt_connect return %d\n", err);
if (client.conn != NULL)
{
altcp_abort(client.conn);
client.conn = NULL;
}
memset(&client, 0, sizeof(client));
}
}
else if (!netif_is_link_up(&gnetif))
{
xEventGroupClearBits(mqttSendEventGroup, MQTT_SEND_EVENT_RUN_BIT);
mqtt_disconnect(&client);
if (client.conn != NULL)
{
altcp_abort(client.conn);
client.conn = NULL;
}
memset(&client, 0, sizeof(client));
osDelay (100);
}
else
{
xEventGroupSetBits(mqttSendEventGroup, MQTT_SEND_EVENT_RUN_BIT);
}
// LwIP heap (MEM_SIZE)
printf("LwIP heap: used: %u / %u bytes (max used: %u bytes)\n",
lwip_stats.mem.used,
lwip_stats.mem.avail,
lwip_stats.mem.max);
// FreeRTOS heap
printf("FreeRTOS heap: current free: %u bytes, minimum ever free: %u bytes\n",
xPortGetFreeHeapSize(),
xPortGetMinimumEverFreeHeapSize());
printf("LwIP pools (current / max / avail):\n");
printf(" PBUF : %u / %u / %u\n",
lwip_stats.memp[MEMP_PBUF]->used,
lwip_stats.memp[MEMP_PBUF]->max,
lwip_stats.memp[MEMP_PBUF]->avail);
printf(" TCP_PCB : %u / %u / %u\n",
lwip_stats.memp[MEMP_TCP_PCB]->used,
lwip_stats.memp[MEMP_TCP_PCB]->max,
lwip_stats.memp[MEMP_TCP_PCB]->avail);
printf(" TCP_SEG : %u / %u / %u\n",
lwip_stats.memp[MEMP_TCP_SEG]->used,
lwip_stats.memp[MEMP_TCP_SEG]->max,
lwip_stats.memp[MEMP_TCP_SEG]->avail);
printf(" ALTCP_PCB : %u / %u / %u\n",
lwip_stats.memp[MEMP_ALTCP_PCB]->used,
lwip_stats.memp[MEMP_ALTCP_PCB]->max,
lwip_stats.memp[MEMP_ALTCP_PCB]->avail);
UBaseType_t stackLeft = uxTaskGetStackHighWaterMark(NULL);
printf("Free stack space MqttConnectTask: %lu words (%lu bytes)\n", stackLeft, stackLeft * sizeof(StackType_t));
osDelay(5000);
}
}Everything works perfectly, but once every few hours the following appears in the log:
LwIP heap: used: 19708 / 36864 bytes (max used: 24452 bytes)
FreeRTOS heap: current free: 12672 bytes, minimum ever free: 10424 bytes
LwIP pools (current / max / avail):
PBUF : 0 / 0 / 16
TCP_PCB : 1 / 2 / 5
TCP_SEG : 0 / 3 / 16
ALTCP_PCB : 2 / 2 / 5
Free stack space MqttConnectTask: 652 words (2608 bytes)
Assertion "unhandled error" failed at line 1079 in ../Middlewares/Third_Party/LwIP/src/apps/altcp_tls/altcp_tls_mbedtls.c
LwIP heap: used: 22300 / 36864 bytes (max used: 24452 bytes)
FreeRTOS heap: current free: 12672 bytes, minimum ever free: 10424 bytes
LwIP pools (current / max / avail):
PBUF : 0 / 0 / 16
TCP_PCB : 1 / 2 / 5
TCP_SEG : 4 / 5 / 16
ALTCP_PCB : 2 / 2 / 5
Free stack space MqttConnectTask: 652 words (2608 bytes)That is, before the message "Assertion "unhandled error" failed at line 1079" appears, there are 0 TCP_SEG in use and 19708 bytes used from the LwIP heap.
After the error, I see 2 TCP_SEG in use and 22300 bytes used from the heap — and this memory is never freed.
After 5, 10, or 20 hours, the same error happens again, and these values increase further. This continues until all available TCP_SEG or heap memory is exhausted, at which point the task simply hangs and stops the data transfer.
At line 1079 in altcp_tls_mbedtls.c, there's only this line:
LWIP_ASSERT("unhandled error", 0);
return ERR_VAL;This error is not handled by LwIP in any way, so the memory is not freed, leading to a memory leak.
I tried disconnecting and re-establishing the connection, replacing the lines above with the following:
LWIP_DEBUGF(ALTCP_MBEDTLS_DEBUG, ("mbedtls_ssl_write failed: %d\n", ret));
if (conn)
{
altcp_abort(conn);
}
return ERR_ABRT;Has anyone encountered a similar issue?
There are many reports about MQTT + mbedTLS hanging after some time, but I haven’t found any working solution yet.