STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32Cube - Barebone FreeRTOS + Lwip on F207

Posted on April 16, 2014 at 20:17Hello to all, I just set up a bare bone project for my F207VC custom board using the new STM32Cube. The board is tested and it is working perfectly with FreeRTOS 6.1.0 and Lwip 1.3.2. The used PHY is a Micrel KSZ8051...

abrous3d by Associate II
  • 3557 Views
  • 7 replies
  • 0 kudos

USB (VCP) and EXTI together dont work

Posted on April 11, 2014 at 18:21Hello All,         I am using the STM32F4 discovery board. I am using USB as a VCP and EXTI for detecting the rising edge of my signal.        The USB and the EXTI work good when operated independently but don't work...

USB Mouse problem on STM32F105

Posted on April 14, 2014 at 11:13Hi to all! I need to work with USB mouse on F105 processor. I used latest USB host-device lib - STM32_USB-Host-Device_Lib_V2.1.0, little rework it: 1. Remove STM3210C-EVAL's display, I have my own display, different ...

hd44780 by Associate
  • 1085 Views
  • 1 replies
  • 0 kudos

STM32F205RF with STM32CubeMX and USB

Posted on April 09, 2014 at 19:54HiI am fighting with USB again.Situation :STM32F205RF in NetDuino2 (schematic is here - http://netduino.com/netduino2/schematic.pdf)Code generated with CubeMX- first page : http://imtp.me/7ga902dr0- clock page : http...

voltr by Associate II
  • 1368 Views
  • 2 replies
  • 0 kudos

STM32F10x + FatFs issue

Posted on April 09, 2014 at 01:52 Hi All, I am new to this community so if I have posted this in the wrong place then please let me know. I have a STM32 Discovery board which I am trying to log data onto a SD card through SPI. I am...

Jump address to choose one of 2 binary in flash

Posted on April 03, 2014 at 17:49Hello, I'm trying to create a bootloader into the component STM32f106RDT with 384KO of Flash. I have mapped the memory like this: 0x08000000 - 0x0802DFFF for main software (first binary) 0x0802F000 - 0x08030FFF reser...

tommelou by Associate II
  • 5984 Views
  • 22 replies
  • 0 kudos

HID Report Descriptor Contains Wrong Byte

Posted on April 09, 2014 at 14:45I've got a USB HID device based on a STM32F427 that can be set up to run as either FS or HS USB. When I use FS, all is well. However, when I use HS (which uses the same descriptor), the report descriptor contains one...

jvavra by Associate III
  • 1328 Views
  • 2 replies
  • 0 kudos