STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Stm324x9I-Eval Ethernet Link Software Interrupt

Posted on September 23, 2014 at 13:04Hello,Kindly guide me in resolving the following issue.I am working on STM324x9I-Eval board Ethernet example using LwIP example.On connecting/disconnecting the Ethernet cable from connector CN10 on the board, I w...

jagdish by Associate II
  • 1734 Views
  • 3 replies
  • 0 kudos

STM32L1: IAP via USB

Posted on September 11, 2014 at 23:17Hello, i'd like to extend my STM32L151 device by adding USB bootloading capability. I searched for documentation and examples, but I got the impression that neither of it exists in a complete fashion. To me it se...

mk299 by Associate III
  • 2440 Views
  • 5 replies
  • 0 kudos

STM32F103RB - USB - Packet memory too small

Posted on September 19, 2014 at 14:33Hi All. I'm working on a project which needs to send and receive audio stream with the size of packet  - 288 bytes one way,  - 576 bytes both ways. Problem is that the Packet Memory is only 512 bytes long and I h...

miki_pf by Associate
  • 1026 Views
  • 1 replies
  • 0 kudos

f_open directory name from variable

Posted on September 18, 2014 at 11:32I'm using a STM32F4  microcontroller witch FatFS library and I'm trying to write a file on an USB OTG drive. I'm using the f_open function and it works fine like thatif(f_open(&fileW, ''0:\\Folder\\INFO.TXT'',FA_...

Lori B. by Associate III
  • 2233 Views
  • 4 replies
  • 0 kudos

STM32Cube hangs when generating code from project

Posted on September 16, 2014 at 06:35Hello, I'm trying to use STM32Cube to generate an IAR project from a 'Cube project configuration for the STM32F405. STM32Cube is installed, and will run, and will download the latest libraries. However when I pre...

geof by Associate II
  • 1052 Views
  • 1 replies
  • 0 kudos

STM32F042K6 flash loader problem

Posted on September 11, 2014 at 14:33Hi,We started to use SMT32F042K6 microcontroller. I need to download program via serial port. So I am tring to use flash loader demonstrator v2.6.0.First of all, I connected my board to PC via FTDI virtual com po...

murat1 by Associate
  • 1776 Views
  • 1 replies
  • 0 kudos

USB CDC Example for DISCO429 Board

Posted on September 11, 2014 at 13:01Hi !I have taken latest Cube4.3.1 and FW package 1.3.0.I have created USB Device VCP example for DISCO429 board and it dosn't work.I can see serial port is appears with yellow triangle in DeviceManager.In forum I...

yevgen by Associate II
  • 1572 Views
  • 3 replies
  • 0 kudos

STM32 USB FS Bulk In speed tuning

Posted on September 10, 2014 at 00:55Using STM32Cube_FW_F4_V1.1.0 on STM32F401 I am trying to maximize data from host to stm on FS bulk endpoint.  Using a 64 byte Rx buffer, I can only get about 5 MBps, as the interrupt and setup for next Rx buffer ...

cpmh1 by Associate II
  • 2333 Views
  • 2 replies
  • 0 kudos