STM32Cube hangs when generating code from project
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-09-15 9:35 PM
Posted on September 16, 2014 at 06:35
Hello,
I'm trying to use STM32Cube to generate an IAR project from a 'Cube project configuration for the STM32F405. STM32Cube is installed, and will run, and will download the latest libraries. However when I press the ''generate source code based on user settings'' button, a box comes up with the message ''Generating user source code...'' and the program just hangs there. I've let it run for over an hour. The only way I can stop the program is to <ctrl><alt><del> and stop the process. When I do that a warning window pops up with the message ''The system cannot end this program because it is waiting for a response from you.'' However there is no such window open for me to respond to. Has someone else seen this problem and found a solution? Many thanks in advance, Geof #stm32cube-bug
Labels:
- Labels:
-
STM32Cube MCU Packages
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2014-09-17 9:06 PM
Posted on September 18, 2014 at 06:06
Well, I found a workaround...
Simply install Cube on a different computer, generate the project there, then send it back to the compute I want to use it on. Sneakers will never be obsolete. :)