STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Cube0 - USB - CustomHID: Report Size

Posted on May 11, 2015 at 13:23 Hi, I got a question concerning the Cube USB library used on the L0 series. I am trying to implement the CustomHID class provided in the USB library. I am developing on the STM32L053 discovery board. ...

STM32L0 USB CUSTOMHID Bidirectional

Posted on November 03, 2015 at 13:26Hi guys, I am working on a solution to implement generic bidirectional data transfer over the USB interface. I am using the current CubeL0 library (version 1.3.0) and the USB library provided in this package. I im...

STM32F4, USB OTG

Posted on November 04, 2015 at 20:22 I have a target application using the STM32F405. On this board I have a USB port. To get started, I found some sample code written by someone for the STM32F4 Discovery board with a few lines of code for main, and...

STM32 F429 USB CDC vs USB MSD with USB FS

Posted on October 29, 2015 at 13:58Hello all,I have a strange question regarding speed od USB CDC and USB MSD driver for STM32F429.I implemented USB MSD + eMMC with FatFS support and I am getting 0.51 MB/s write and 0.69 MB/s read speed results with...

FreeRTOS + FatFs (STM3240G) -> FR_DISK_ERR

Posted on December 04, 2014 at 14:54 Hello, I've modified FatFs_uSD_RTOS example to write in a loop (32k files), which works fine on its own (Task SDCardStream()). When I add another task Process() which only has a calculation loop: sta...

ariel2 by Associate II
  • 3843 Views
  • 7 replies
  • 0 kudos

STM32F40G-EVAL Ethernet Lwip IAP application

Posted on October 30, 2015 at 20:20Hello, I am trying to implement the LWIP_IAP application on the STM32f40g EVAL board. After compiling the project, the program size turns out to be as follows. Program Size: Code=28150 RO-data=3114 RW-data=260 ZI-d...

bhatia by Associate
  • 1314 Views
  • 1 replies
  • 0 kudos

Cortex m0+ eeprom

Posted on October 30, 2015 at 15:55Hello, I use a Cortex M0 + to develop an application. With this cortex, I need to write in memory and this take 12 seconds by bytes. Could someone tell me if this is normal or not? thanks in advance . I'm using...

SDIO vs SPI

Posted on December 09, 2013 at 17:03I am using STM32f4 ,fat fs & SPI mode to interface to SD card every thing works fine .but i want to use DMA to increase read performance.should i go for SDIO to achieve a little more speed or is there any way to t...