cancel
Showing results for 
Search instead for 
Did you mean: 

stm32 USB OTG mass storage device enumeration failed

danashevskiy
Associate II
Posted on November 03, 2015 at 10:20

In my device based on stm32f107 connectivity line model i use

http://www.st.com/web/en/catalog/tools/PF257882#

http://www.st.com/web/en/catalog/tools/PF257882#

. When i connect device to the PC with Windows 7, last one recognizes stm32f107 as ''Unknown Device''. This means that USB enumeration process has been failed and i can't understand ''why?''

The early interrupt routine can be found in usb_dcd_int.c of standart library.

uint32_t USBD_OTG_ISR_Handler (USB_OTG_CORE_HANDLE *pdev)

{

USB_OTG_GINTSTS_TypeDef gintr_status;

uint32_t retval = 0;

if

(USB_OTG_IsDeviceMode(pdev))

/* ensure that we are in device mode */

{

gintr_status.d32 = USB_OTG_ReadCoreItr(pdev);

if

(!gintr_status.d32)

/* avoid spurious interrupt */

{

return

0;

}

if

(gintr_status.b.outepintr)

{

retval |= DCD_HandleOutEP_ISR(pdev);

}

if

(gintr_status.b.inepint)

{

retval |= DCD_HandleInEP_ISR(pdev);

}

if

(gintr_status.b.modemismatch)

{

USB_OTG_GINTSTS_TypeDef gintsts;

/* Clear interrupt */

gintsts.d32 = 0;

gintsts.b.modemismatch = 1;

USB_OTG_WRITE_REG32(&pdev->regs.GREGS->GINTSTS, gintsts.d32);

}

if

(gintr_status.b.wkupintr)

{

retval |= DCD_HandleResume_ISR(pdev);

}

if

(gintr_status.b.usbsuspend)

{

retval |= DCD_HandleUSBSuspend_ISR(pdev);

}

if

(gintr_status.b.sofintr)

{

retval |= DCD_HandleSof_ISR(pdev);

}

if

(gintr_status.b.rxstsqlvl)

{

retval |= DCD_HandleRxStatusQueueLevel_ISR(pdev);

}

if

(gintr_status.b.usbreset)

{

retval |= DCD_HandleUsbReset_ISR(pdev);

}

if

(gintr_status.b.enumdone)

{

retval |= DCD_HandleEnumDone_ISR(pdev);

}

if

(gintr_status.b.incomplisoin)

{

retval |= DCD_IsoINIncomplete_ISR(pdev);

}

if

(gintr_status.b.incomplisoout)

{

retval |= DCD_IsoOUTIncomplete_ISR(pdev);

}

#ifdef VBUS_SENSING_ENABLED

if

(gintr_status.b.sessreqintr)

{

retval |= DCD_SessionRequest_ISR(pdev);

}

if

(gintr_status.b.otgintr)

{

retval |= DCD_OTG_ISR(pdev);

}

#endif

}

return

retval;

}

 In debug mode i've found that switch process stops in DCD_HandleEnumDone_ISR.   static

uint32_t DCD_HandleEnumDone_ISR(USB_OTG_CORE_HANDLE *pdev)

{

USB_OTG_GINTSTS_TypeDef gintsts;

USB_OTG_GUSBCFG_TypeDef gusbcfg;

USB_OTG_EP0Activate(pdev);

/* Set USB turn-around time based on device speed and PHY interface. */

gusbcfg.d32 = USB_OTG_READ_REG32(&pdev->regs.GREGS->GUSBCFG);

/* Full or High speed */

if

( USB_OTG_GetDeviceSpeed(pdev) == USB_SPEED_HIGH)

{

pdev->cfg.speed = USB_OTG_SPEED_HIGH;

pdev->cfg.mps = USB_OTG_HS_MAX_PACKET_SIZE ;

gusbcfg.b.usbtrdtim = 9;

}

else

{

pdev->cfg.speed = USB_OTG_SPEED_FULL;

pdev->cfg.mps = USB_OTG_FS_MAX_PACKET_SIZE ;

gusbcfg.b.usbtrdtim = 5;

}

USB_OTG_WRITE_REG32(&pdev->regs.GREGS->GUSBCFG, gusbcfg.d32);

/* Clear interrupt */

gintsts.d32 = 0;

gintsts.b.enumdone = 1;

USB_OTG_WRITE_REG32( &pdev->regs.GREGS->GINTSTS, gintsts.d32 );

return

1;

}   Here host should give device address and check it's descriptors. And after that there are no actions. What can be the reason of failing enumeration process?BTW i have flash chip in device and i didn't mounted any filesystems on it.

UPDATE: After checking the signal processes with oscilloscope i've found that data flows only in one way. PC sends some commands, i think stm32 even reads this input data with

USB_OTG_READ_REG32()

and then tries to send data with

USB_OTG_WRITE_REG32()

but i see no signal on oscilloscope display.

#usb #stm32f10x

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0