STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Boot1 pin left floating

Posted on April 19, 2016 at 14:38Hi,I am now working on a design with stm32l, the BOOT1 pin was left floating in this design, Is that a valid configuration? Does BOOT1 have a built in pull down/up resistor, or is it an unstable configuration?Thanks ...

udilevy by Associate II
  • 1486 Views
  • 2 replies
  • 0 kudos

STM32L4 ST bootloader I2C mode

Posted on April 19, 2016 at 02:54I am studying the feasibility that using ST ROM bootloader I2C mode to program my application. Here have several questions: 1) does the STM32L4 bootloader supports the I2C? I find a AN2606 doc, but it does not state ...

jiangpen by Associate II
  • 824 Views
  • 1 replies
  • 0 kudos

STM32L0x Boot0

Posted on April 15, 2016 at 13:45Fellows on some STM32L0 (STM32L011x3/4 TSSOP2) Boot0 is also  PB9 on others (STM32L031x4/6 TSSOP2) only Boot0. Is this not allways the same for a STM32 familiy like STM32L0x? Is that correct? I think on we need as mu...

felix2 by Associate II
  • 3330 Views
  • 6 replies
  • 0 kudos

STM32F411RE cmsis led don't turn off

Posted on April 10, 2016 at 19:46Hi, I've got problem with code. LED on my board STM32F411RE don't turn off when I'm using cmsis library but in HAL or StdPeriph it works. &sharpinclude ''stm32f4xx.h'' &sharpinclude ''core_cm4.h'' int main(void) {   ...

lukarzmen by Associate II
  • 1992 Views
  • 7 replies
  • 0 kudos

Real bug in the USB CDC

Posted on September 15, 2014 at 14:39USBD_CDC_TransmitPacket() function contains a bug: it sets the 'transmission in progress' flag AFTER starting the actual transmission, so if the 'transmission done' interrupt happens too early, the flag will be ...

ksa by Associate
  • 3882 Views
  • 9 replies
  • 0 kudos

USB on STm32F411RE

Posted on April 07, 2016 at 11:07Hi,I'm trying to handle a printer via USB with my http://www.st.com/web/en/catalog/tools/PF260320 but I'm facing a problem. Indeed, when my board send the first request for the enumeration, it goes in a waiting time ...

quentin23 by Associate II
  • 1980 Views
  • 2 replies
  • 0 kudos

2 UART running in FreeRTOS

Posted on April 07, 2016 at 15:11Hi, I use 2 UART ports: UART1 for WiFi and UART4 for debug output. My goal is to send to UART4 data I received on UART1. When I use only 1 UART, it works (UART4), everything I typed on keyboard, returned back. I impl...