USB on STm32F411RE
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-04-07 2:07 AM
Posted on April 07, 2016 at 11:07
Hi,
I'm trying to handle a printer via USB with my but I'm facing a problem. Indeed, when my board send the first request for the enumeration, it goes in a waiting time forever :phost -> gState = HOST_ENUMERATIONphost -> EnumState = ENUM_IDLEphost -> RequestState = CMD_WAITandphost -> Control -> state = CTRL_SETUP_WAITWhen I check the DP and DM line, there are indeed communication between my printer and the board but I don't know what the message means.For the Hardware, I have (sorry but there is a bug when I try to put a picture or a code block...). The LP2980-5 is a linear regulator supplied with 10V.For the Code, I'm inspired by a MSC_HOST application from STM324xG_Eval. Here the main part of usb_conf.c (I attach the complete file just in case):void HAL_HCD_MspInit(HCD_HandleTypeDef *hhcd){ GPIO_InitTypeDef GPIO_InitStruct; /* Configure USB FS GPIOs */ __HAL_RCC_GPIOA_CLK_ENABLE(); //__HAL_RCC_GPIOH_CLK_ENABLE(); GPIO_InitStruct.Pin = (GPIO_PIN_11 | GPIO_PIN_12); GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF10_OTG_FS; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); GPIO_InitStruct.Pin = GPIO_PIN_6; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); /* Enable USB FS Clocks */ __HAL_RCC_USB_OTG_FS_CLK_ENABLE(); /* Set USBFS Interrupt to the lowest priority */ HAL_NVIC_SetPriority(OTG_FS_IRQn, 5, 0); /* Enable USBFS Interrupt */ HAL_NVIC_EnableIRQ(OTG_FS_IRQn);}USBH_StatusTypeDef USBH_LL_Init(USBH_HandleTypeDef *phost){ /* Set the LL driver parameters */ hhcd.Instance = USB_OTG_FS; hhcd.Init.Host_channels = 11; hhcd.Init.dma_enable = 0; hhcd.Init.low_power_enable = 0; hhcd.Init.phy_itface = HCD_PHY_EMBEDDED; hhcd.Init.Sof_enable = 0; hhcd.Init.speed = HCD_SPEED_FULL; /* Link the driver to the stack */ hhcd.pData = phost; phost->pData = &hhcd; /* Initialize the LL Driver */ HAL_HCD_Init(&hhcd); USBH_LL_SetTimer(phost, HAL_HCD_GetCurrentFrame(&hhcd)); return USBH_OK;}USBH_StatusTypeDef USBH_LL_DriverVBUS(USBH_HandleTypeDef *phost, uint8_t state){ if(state == 0) { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_RESET); } else { HAL_GPIO_WritePin(GPIOA, GPIO_PIN_6, GPIO_PIN_SET); } HAL_Delay(200); return USBH_OK; }Except for the Vbus pin, I didn't change much. I although tried to use the mass storage class with a usb stick to be sur the problem didn't come from my printer class. It didn't change anything as expected.Has anyone succeed to use this board as USB host ? For the others, is there a obvious problem that I don't get ?Thank you. #msc #usb #host
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-04-07 12:02 PM
Posted on April 07, 2016 at 21:02
Hi hivert,
On your schematic, the connection of D+/D- lines is swapped. The right connection is, PA11 -- D- (DM) PA12 -- D+ (DP) > Has anyone succeed to use this board as USB host ? I tested CubeMX MSC (Mass-Storage Class) host on NUCLEO-F411RE board. Generated code worked for a USB stick without any change, at least on these steps. enumeration and initial MSC setup - GetMaxLUN - INQUIRY - TEST UNIT READYY - READ CAPACITY 10 (observed on a hardware bus analyzer) CubeMX: 4.0 STM32Cube_FW_F4_V1.0 I attached CubeMX setting file (zip) to this post. As of the hardware connection, 1) clock source - MCO from ST-Link My NUCLEO-F411RE (MB1136 C-02 revision) has default MCO connection from on-board ST-Link. If your board would be C-01 revision, solder the jumpers, following to section ''5.6.1 OSC clock supply'' of the NUCLEO64 manual ( ). 2) Connection to USB type-A connectorNUCLEO-F411RE type-A
PA12 CN10 pin12 -- D+ PA11 CN10 pin14 -- D- +5V CN7 pin18 -- VBUS (5V) GND CN10 pin 9 -- GND Try this one as the start point of your project. Tsuneo ________________ Attachments : cubemx_nucleo_f411re_msc_host.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0bO&d=%2Fa%2F0X0000000bb0%2FtYhjRvfFODfmTrpTX8Go0nahX_0j0l8XKoX7vyGef_A&asPdf=falseOptions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2016-04-08 6:48 AM
Posted on April 08, 2016 at 15:48
Hi Tsuneo and thank you a lot for your help. Its works perfectly fine now and my printer is detected.
I'm not quite sure what was wrong before but nevermind.PS : I see you are the one who have helped for printer class [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/USB%20printer%20class&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=1210]here so double-thanks for you.