STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32F105 / FS Bulk and Isochronous transfers

Posted on April 19, 2016 at 16:30Hi,I have a project that voice and parameter data will be transferred through Pc to STM32 and STM32 to PC. I want to use CDC to transfer parameters and isochronous to transfer voice. Is it possible to use isoc and bu...

Boot1 pin left floating

Posted on April 19, 2016 at 14:38Hi,I am now working on a design with stm32l, the BOOT1 pin was left floating in this design, Is that a valid configuration? Does BOOT1 have a built in pull down/up resistor, or is it an unstable configuration?Thanks ...

udilevy by Associate II
  • 1448 Views
  • 2 replies
  • 0 kudos

STM32L4 ST bootloader I2C mode

Posted on April 19, 2016 at 02:54I am studying the feasibility that using ST ROM bootloader I2C mode to program my application. Here have several questions: 1) does the STM32L4 bootloader supports the I2C? I find a AN2606 doc, but it does not state ...

jiangpen by Associate II
  • 798 Views
  • 1 replies
  • 0 kudos

STM32L0x Boot0

Posted on April 15, 2016 at 13:45Fellows on some STM32L0 (STM32L011x3/4 TSSOP2) Boot0 is also  PB9 on others (STM32L031x4/6 TSSOP2) only Boot0. Is this not allways the same for a STM32 familiy like STM32L0x? Is that correct? I think on we need as mu...

felix2 by Associate II
  • 3202 Views
  • 6 replies
  • 0 kudos

STM32F411RE cmsis led don't turn off

Posted on April 10, 2016 at 19:46Hi, I've got problem with code. LED on my board STM32F411RE don't turn off when I'm using cmsis library but in HAL or StdPeriph it works. &sharpinclude ''stm32f4xx.h'' &sharpinclude ''core_cm4.h'' int main(void) {   ...

lukarzmen by Associate II
  • 1887 Views
  • 7 replies
  • 0 kudos

Real bug in the USB CDC

Posted on September 15, 2014 at 14:39USBD_CDC_TransmitPacket() function contains a bug: it sets the 'transmission in progress' flag AFTER starting the actual transmission, so if the 'transmission done' interrupt happens too early, the flag will be ...

ksa by Associate
  • 3775 Views
  • 9 replies
  • 0 kudos

USB on STm32F411RE

Posted on April 07, 2016 at 11:07Hi,I'm trying to handle a printer via USB with my http://www.st.com/web/en/catalog/tools/PF260320 but I'm facing a problem. Indeed, when my board send the first request for the enumeration, it goes in a waiting time ...

quentin23 by Associate II
  • 1947 Views
  • 2 replies
  • 0 kudos