STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Usb hid host problem

Posted on July 21, 2014 at 23:15I am interfacing a standard usb keyboard with stm32f4 discovery board. I am using a usb host library which are provided by st. Now the keyboard is successfully connected with discovery board and all keys are decoded s...

FatFS SDIO DMA write speed

Posted on July 23, 2014 at 14:28Hello.I'm trying to get more SD card write performance with STM32F207ZET6 + SDIO + DMA + FatFS.I'm using Kingston 8GB MicroSDHC 4 class. I formatted it with SD Formatter tool. File system FAT32 with 32KB clusters.Writ...

pbox by Associate II
  • 2993 Views
  • 5 replies
  • 0 kudos

USB library stalls while waiting for response

Posted on July 21, 2014 at 20:25 Hello, I'm currently working with an STM32F215 mcu and I'm attempting to write a test program with the USB-Host-Device Library V.2.1.0. The goal of this test project is to program the STM32F215 as a host c...

STM32CubeMX for F4 PolarSSL

Posted on July 17, 2014 at 23:10I've installed STM32CubeMX to see how it would work for a new board I'm planning on building.  Is there anything special I have to do to make PolarSSL show up in the middleware section?  I see LWIP, and can enable it,...

jwormsley by Associate III
  • 541 Views
  • 2 replies
  • 0 kudos

STM32F4 Cube and FreeRTOS Don't Cooperate

Posted on June 16, 2014 at 21:08Hi, I'm having a very difficult time getting FreeRTOS v8 to run with CUBE/HAL. I started out using CUBE to generate a basic example for an ADC input configuration, and a timer that will count up (or down) and execute ...

Can't find USB Host library for STM32 F3 series

Posted on July 10, 2014 at 06:59Hi - been checking for a while now, but I can't find any ''USB Host'' library for STM32 F3 series (I'm specifically using STM32F303VC and I have a STM32F3Discovery board).I only found: ''USB Device'' for F3 included...

maggie by Associate III
  • 921 Views
  • 4 replies
  • 0 kudos

STM32F407 USB Disconnect detected interrupt problem

Posted on July 15, 2014 at 07:22Hi,I am presently working on STM32F407 USB, for my understanding i am referring the RM0090 Reference manual.In that manual for USB OTG FS, Global interrput register (GINTSTS) 29 bit as DISCINT bit at there they given ...

chandu1 by Associate II
  • 693 Views
  • 1 replies
  • 0 kudos

HAL Timer Module - read & set counter value

Posted on July 16, 2014 at 12:22In the old standard drivers, you could use TIM_GetCounter(TIM2) and  TIM_SetCounter(TIM2, 0) to read or modify the timer counter values. Is there a similar thing within the HAL drivers? I can't seem to find any replac...

rajpaged by Associate II
  • 5498 Views
  • 1 replies
  • 0 kudos