STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

trouble shooting USB MSC device firmware

Posted on March 26, 2016 at 16:57Hello,I could use some help. I have to implement a USB Mass Storage device on a STM32L476. The final hardware is not ready jet, so I started by using a stm32476RG Nucleo board. I�ve started with the MSC_Standalone ex...

torsten2 by Associate II
  • 5454 Views
  • 11 replies
  • 0 kudos

audio ringing/crosstalk

Posted on June 07, 2016 at 16:54I posted on the eval forum but after further experiments trying here. I'm using the STM32F746G Discovery.  I'm using the audio_loopback.c demo slightly modified to use line inputs instead of mics.  I get lots of cross...

dennis by Associate II
  • 1742 Views
  • 2 replies
  • 0 kudos

Interruption problem with SPI cubemx

Posted on July 11, 2016 at 17:18 Hello, I have a reception problem with SPI interruption, I only triggers once the interruption and my array is filled with this one character who repeats.. Thank you for your help. main.c /* ...

ibrahim by Associate II
  • 1123 Views
  • 1 replies
  • 0 kudos

STM32 Cube USB VCP

Posted on August 18, 2014 at 14:31Hello,I'm trying to get a virtual com port working on the stm32f4 discovery board. This is something that I've managed to do in the past using the old USB libraries and std peripheral libraries. However, since st is...

CMSIS in Discovery board example

Posted on July 11, 2016 at 14:48Hi, I'm using Discovery Board with USB_Device\MSC_Standalone\MDK-ARM project. I'm trying to read sd card written with my Android phone. The result is the image attached. What is the problem? Thanks #usb #sdcard #cm...

0690X00000605IFQAY.png

USB get feature reports with HAL device library?

Posted on August 28, 2015 at 21:03Hello, up to now I used the SPL USB device code and I'd like to switch to the HAL/Cube version now. Unfortunately that only supports setting feature reports. But I'd also like to get feature reports from the device....

mk299 by Associate III
  • 2383 Views
  • 5 replies
  • 1 kudos

STM32 HAL_SPI_Transmit/Receive limitation

Posted on July 07, 2016 at 23:41version F4, 1.12 I am interfacing SPI to flash. calling HAL_SPI_Transmit or Receive alone disables SPI_DIRECTION_2LINES. I have to re-initialize it after each call. When using HAL_SPI_TransmitReceive. I have to specif...

alsaleem by Associate II
  • 1526 Views
  • 2 replies
  • 0 kudos

Issues with STM32F4 USB bulk transfer (MIDI)

Posted on December 07, 2012 at 18:47Hi all,I'm working on an application for the STM32F4 where I need a USB MIDI device class. I've started with the STM USB library and, looking at the CDC and Audio class examples, have come up with a MIDI device th...