cancel
Showing results for 
Search instead for 
Did you mean: 

Transmit data between two STM3240G Eval Boards via Internet/LAN through Ethernet peripheral

bharcooldude
Associate
Posted on July 11, 2016 at 09:43

I am trying to establish a connection between two STM3240G eval boards via Ethernet peripheral. I downloaded the STM32F4 example codes and tried running HTTP server raw code. The documentation asks me to configure a remote PC to a static IP address. I am unable to proceed forward here. Also when the board is connected to a LAN, it is supposed to show the log data and assigned IP address to display on the onboard LCD display, but it stays blank. Any idea why? I've attached the readme.txt file given along with the example for reference.

#stm3240g-ethernet
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0