cancel
Showing results for 
Search instead for 
Did you mean: 

IpWayStudio Eclipse IDE. TCP/IP and touch screen applications on STM32 Discoveries

ingdm
Associate

Posted on July 12, 2016 at 11:20

Dear users,

I have developed the IpWayStudio IDE based on Eclipse. You can get it here: /external-link.jspa?url=https%3A%2F%2Fsourceforge.net%2Fprojects%2Fipway%2F

.

You can find some demo applications inside. All you need to do is:

- downalod IpWayStudio from here: 

/external-link.jspa?url=https%3A%2F%2Fsourceforge.net%2Fprojects%2Fipway%2F

- get a discovery board among the following: 32F746GDISCOVERY, 32F769IDISCOVERY or NUCLEO-H743ZI .

- runni ng your application.

You will find a Quick Start Guide about IpWayStudio and an application note of the demos.

The demos are based on IpWay/HOST free Tcp/Ip Stack Library, moreover they make also use of other software component as touch screen library and so on.

The project is frequently updated, stay tuned!

Enjoy it!!!

Best Regards.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Nesrine M_O
Lead II
Posted on July 13, 2016 at 15:02

Hi di_martino.giovanni,

Thank you for sharing your application with us.Hope that this will be helpful for forum users.

-Syrine-