STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Multichannel ADC reading

Posted on August 16, 2016 at 18:31Hi,I am trying to read two adc channels number 10 and 11 with cubemx output. I can read the 10th channel with this code:HAL_ADC_Start(&hadc1);HAL_ADC_PollForConversion(&hadc1,10);value_adc=HAL_ADC_GetValue(&hadc1);H...

er3481 by Senior
  • 4878 Views
  • 9 replies
  • 1 kudos

STM32F746G- usb device mass storage with RTOS

Posted on July 19, 2016 at 16:03hi,      i have compiled and flashed the USB mass storage standalone project from STM32Cube_FW_F7_V1.1.0 STM32F746G MCU it works fine. but i have linked the same files with my project with RTOS now it showing in compu...

rajesh23 by Associate II
  • 3795 Views
  • 9 replies
  • 0 kudos

Boot into multiple main applications?

Posted on August 16, 2016 at 15:30I currently have my own bootloader running with a main application on a STM32F429ZIT.  The internal flash memory is broken down into 3 sections:1. Bootloader2. Main Application (Bank A)3. Temporary storage for new u...

Dual boot on STM32F427?

Posted on August 13, 2016 at 11:59Hello,I am rather confused, as I have read software dual boot was only possible in f7.But I recently came across dual bank boot options available on f4 : is it possible to dual boot on f4, in soft real-time?I use th...

maxzor by Associate II
  • 1293 Views
  • 2 replies
  • 0 kudos

HardFault with lwip+freeRTOS and STM32f745

Posted on April 18, 2016 at 11:02Hello, I'm using the lwip stack in combination with FreeRTOS for a http server (Netconn API) and modbus TCP (FreeModbus). I'm using the lwip stack and FreeRTOS from the ''STM32Cube_FW_F7_V1.3.0''. Evriting works grea...

twagner by Associate II
  • 3360 Views
  • 4 replies
  • 0 kudos

lwip+modbus/tcp

Posted on September 03, 2013 at 17:04hello every one .i tried to add modbus/tcp protocol in lwip(in webserver demo). i did it and it worked .but the problem is : if i use modbus/tcp protocol(via modbus poll software) it works correctly and if i use ...

USB-HID-HOST on STM32F407 / STM3240G EVAL

Posted on August 15, 2016 at 20:53Hello, I tried the example on the evaluation-board STM3240G-EVAL with the USB-HID-Host in Standalone mode HS and FS from the CubeF4 examples. The mice is recognised properly. The keyboard seems to work not properly....

ssl85 by Associate
  • 757 Views
  • 0 replies
  • 0 kudos

Full duplex usart data corruption

Posted on August 12, 2016 at 09:52 I'm currently working on a system with 2 STM32, which communicate with each other via a full duplex USART. The chips are a STM32F746VG (we'll call MCU1) and STM32F411CE (MCU2). MCU1 uses t...

USB Host CDC - USB Attached

Posted on August 08, 2016 at 20:36Hello, I generate code using stm32cube to make an USB host CDC. If my device is already plugged, it is not detected. Do you have any solutions to detect it ? Thank you in advance. #stm32-usb-cdc-host-attached

guigui by Associate II
  • 979 Views
  • 1 replies
  • 0 kudos