2016-08-13 2:59 AM
Hello,
I am rather confused, as I have read software dual boot was only possible in f7.But I recently came across dual bank boot options available on f4 : is it possible to dual boot on f4, in soft real-time?I use the f427 chip on a flight controller board for a drone. I wonder if it is possible to switch firmware in-flight...Best regards,Maxime #dual-boot2016-08-13 4:02 AM
The 2MB models have two 1MB banks.
If you fork the code (from a common point in both banks) and clear the caching (ART) swapping the banks while running should be possible. The bank swap is a single bit, and changes the address decode. I'd use a common 16KB loader in the first sector of both banks to achieve this.2016-08-16 8:39 AM
Thank you! Will have a further look into it.