USB-HID-HOST on STM32F407 / STM3240G EVAL
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2016-08-15 11:53 AM
Posted on August 15, 2016 at 20:53
Hello,
I tried the example on the evaluation-board STM3240G-EVAL with the USB-HID-Host in Standalone mode HS and FS from the CubeF4 examples. The mice is recognised properly. The keyboard seems to work not properly. I tested different keyboards and when I plug them in, I can say, they are recognised as a keyboard because the screen shows me that a keyboard is active, but when I press a button on the keyboard, there is no further reaction in the software... What is the problem with the protocol? Do the keyboards have to fullfill any special conditions to work properly with the evalutaion-board? Thanks a lot! #usb-hid-host-keyboard-stm32f4
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0