STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Triple mode ADC with new HAL

Posted on December 02, 2014 at 01:06 Hello, I'm trying to set the ADC(s) of the stm32f407 in triple mode, using DMA for data transfers. Based on the the only available example in the cube package and some old code, written using the stdpheri...

b2527456 by Associate II
  • 2504 Views
  • 10 replies
  • 0 kudos

USB HID - Get Feature Report Asynchronous

Posted on December 02, 2014 at 14:14Hello guys,I am working with the new CubeMX lib on a STM32F4 platform and altough I worked a lot with the ST USB HID implementation/stack it still gives me headaches. I am still new to USB.I am developing an HID d...

STM32F105 + USB

Posted on December 11, 2014 at 18:15 Hello I have a STM32F105RC. I am try use ''STM32_USB-Host-Device_Lib_V2.1.0''. But my PC don't detect my device. I use this defines symbols USE_STDPERIPH_DRIVER STM32F10X_CL ...

lemac by Associate III
  • 746 Views
  • 2 replies
  • 0 kudos

STM32 Custom Bootloader for Stm32VL Discovery

Posted on December 05, 2014 at 12:15Hii,          I am new to the topic of Bootloaders, I am currently writing a custom bootloader for stm32 vl discovery via USART, I am searching for the source codes of the factory Programmed bootloader of stm32, a...

FreeRtTOS Timers running slow on custom board

Posted on December 05, 2014 at 05:20FreeRTOS on Discovery board  one tick = 1 msecFreeRTOS on custom board  one tick = 10 msec   (same code as running on Discovery Board)Uart code Interrupt driven  runs on both boards ADC/DMA Interrupt driven code r...

barry by Associate II
  • 1393 Views
  • 6 replies
  • 0 kudos

STM32F105RC USB HID device

Posted on December 09, 2014 at 18:12HelloI was using a nucleo F103 like explain in the thread ''Nucleo-F103RB + USB''.Now I have the finish board. In the finish board i am using a STM32F105RC.SO i change the compiler from STM32F10X_MD to STM32F10X_C...

lemac by Associate III
  • 378 Views
  • 0 replies
  • 0 kudos

g

Posted on December 03, 2014 at 22:44g #hal_uart_error_pe-uart-parity

hossam by Associate II
  • 778 Views
  • 3 replies
  • 0 kudos

STM32F411, STM32CubeMX, USB Device for CDC

Posted on November 26, 2014 at 08:09STM32F411RCTx, LQFP64When using STM32CubeMX Ver4.4 to generate USB Device only code for CDC class, initialization is fine but cannot connect to PC (host).The STM32CubeMX generated code also has same problem as MDK...

bardeen by Associate
  • 930 Views
  • 2 replies
  • 0 kudos

stm32f207 usb only multiple of 64 bytes can be send

Posted on April 10, 2013 at 10:04change by stm32 usb device VCP example: my send function: uint16_t VCP_DataTx (uint8_t* Buf, uint32_t Len) {  uint8_t i;  for (i=0;i<64;i++)    //only multiple of 64 bytes can be send   {  APP_Rx_Buffer[APP_Rx_ptr_in...

easylwl by Associate II
  • 1538 Views
  • 7 replies
  • 0 kudos